Part Number: LMK1C1104 Other Parts Discussed in Thread: CDCLVC1104 , Hi team
My customer is considering about replacing their current Renesas solution(ICS2304NZG-1LF) to ours, and is currently looking at LMK1C1104 and CDCLVC1104.
They will need some additional…
Part Number: LMK1C1104 Other Parts Discussed in Thread: LMK00334 , LMK00804B , CDCLVC1104 , Hi
We are using LMK1C1104DQFT in our design. Kindly suggest equivalent alternate part for the same.
Part Number: LMK1C1104 Hi team,
customer want to use this on UFS storage application,
can LMK1C1104 still function when VDD is 1.2V, I only see 1.8V in datasheet.
if not, can you recommend other solution that can do,
Regards,
Fred
Part Number: LMK1C1104 Hi,
Our circuit used LMK1C1104 devices. Our processor requires three 50MHz CMOS clocks at 1.8V. The design is as follows. Please help to check whether there is any problem with this design. Thank you very much.
Part Number: LMK1C1104 Hi Team,
Customer is consulting why the output impedance of LMK1C1104DQFT is changed w/ different VDD? Could you pls help explain this? Thanks.
Best,
Stanley
Part Number: LMK1C1104 Other Parts Discussed in Thread: LMK1C1103 , LMK1C1102 Hello,
I have one question regarding the LMK1C1104.
The datasheet specifies that the unused outputs can be left floating, but are there any drawbacks to it compared to having…
Part Number: LMK1C1104 The customer is consulting for solution as a clock buffer.
Input clk frequency 19.2MHz, 1.15V
output 19.2MHz 1.2V
Vdd=1.2V
Do you have a preferred one to promote here?
Thanks for your help
Max
Part Number: LMK1C1104 I am wondering if it is safe to apply a voltage or clock to the CLKIN pin when device is upowered (VDD = 0 V)?
I see that the Absolute Maximum Ratings section says the voltage can be -0.5 to 3.6 V, regardless of VDD, so I am assuming…
Part Number: LMK1C1104 Other Parts Discussed in Thread: CDCV304 , , CDCE949 Hello,
Does the clock input (general all inputs) provide clamping diode(s) to Vdd? Currently we are powering the clock buffer via electronic switch (+3.3V switched). The clock input…