Part Number: LMK1C1108 Hi,
I would like to use a clock buffer to split a trigger pulse to several devices in the same time, of course.
Is it possible to simulate this component : LMK1C1108 with PSpice for TI public version ?
How can I find or add this…
Kengo,
We only have the jitter numbers to provide in PLL (zero-delay) mode.
If zero-delay is not required, then I recommend actually using the LMK1C1108 instead: https://www.ti.com/lit/ds/symlink/lmk1c1108.pdf
The LMK1C1108 will have lower additive jitter…
Part Number: LMK1C1108 Hi Team, The first page of the datasheet shows that the max temperature range of LMK1C1108 is 125 deg C. Page 16 and also the information in the product folder shows 105 deg C. Please confirm which is correct. Thanks, Jonathan
Hello Matthew,
That is correct, the maximum Vin voltage would be 3V in this case. However, the LMK1C1108 would work, as shown in this statement from the data sheet:
Best,
Andrea
Part Number: LMK1C1104 Other Parts Discussed in Thread: LMK1C1108 Tool/software: I am looking for an alternative for LMK1C1104DQFR. I need higher output current and faster rise time.
Please let me know if you have a device that meets these needs.
Hi Rhea,
If you do not have an existing clock signal, I recommend the CDCEL949 clock generator.
If you have an existing clock signal, I would recommend the LMK1C1108 buffer.
Do you have any jitter requirements?
Best, Michael