Part Number: LMK1D2102 Hello team,
I wanted to use LMK1D2101 to convert single ended clock(0.8 Vpp Clipped Sine Wave generated from ASVTX-13-A-19.200MHZ) to differential LVDS Clock. Is it possible to use this device for this purpose ? If yes, can you…
Part Number: LMK1D2102 Other Parts Discussed in Thread: LMK5C33216 , LMK5B12204 I would like to connect the output of the Analog Devices AD9545 oscillator to the input of the LMK1D2102. I am using 1.8V supplies. The AD9545 can be configured to output differential…
Part Number: LMK1D2102 Hi Team,
Good day!
Could you please share us the value of the VTH Value of this device. Our cusotmer is using LMK1D2102RGTR for translating from LVCMOS (single -ended ) signal to two copies of LVDS signal (each of them around 2.5V…
Part Number: LMK1D2102 Tool/software: I would like to use the LMK1D2102 to input a sine wave clock (differential) of about 100 MHz and output an LVDS clock.
From the following questions, it seems possible to input a sine wave, but the noise floor and…
Part Number: DS90UH948-Q1 Other Parts Discussed in Thread: LMK1D2102 Tool/software: Hello,
We are designing device which should implement HDCP repeater mode according to Figure 7-12, p.38 in datasheet. But concerning about signal integrity issues in…
Hello Chen, We have dedicated LVDS buffers. LMK1D2102 family can better meet your needs and its newer part.
LMK1D210x Low Additive Jitter LVDS Buffer datasheet (Rev. B)
The 27MHz input is supported.
I am unsure of what you mean by the skew standard - can…
Part Number: LMK04832 Other Parts Discussed in Thread: LMK1D1204 , LMKDB1102 , SN65LVDS32 , LMK1D1204P , LMK1D2102 Tool/software: Dear Exprts,
Need some advice below:
Referenced to TI’s below app note, figure 13, we are planning to use the below multidrop…
Guohai Lin,
The CDCLVP1102 is a universal input, LVPECL output buffer. We do not offer any 1:2 buffers that have LVDS outputs. But the LMK1D2102 is a dual 1:2 LVDS buffer and the LMK00304 is a 1:4 buffer which can be configured as an LVDS output. With both…
Part Number: LMK1D1204 Other Parts Discussed in Thread: LMK1D2102 , CDCE6214 hi,
customer is searching a clock buffer with below retirements. any suggestions?
supply voltag:1.8v;
Input signal : single-end 125Mhz LVCMOS;
Output signal: differential…