Part Number: LMKDB1108 Tool/software: Hello,
I have a design using LMKDB1108 as a buffer and clock monitor. The clock is suppled to the design from an external piece of equipment. There is an on-bord microcontroller that is responsible for configuring…
Part Number: LMKDB1108 Tool/software: Hello,
I have a design using the LMKDB108Z100RKPT and I cannot get the LOS# on pin 1 to go low when I remove the Clock Input.
Here is the setup:
1) VDDA is at 3.3V,
2) The PWRGD/PWRDN# (pin 12) is at 3.3V…
Part Number: LMKDB1108 Hello team,
On the datasheet, the input clock slew rate is minimum 0.6V/ns when differential clock. Would it be same for single ended clock, if the amplitude is 300mVpp?
Best Regards, Kei Kuwahara
Part Number: LMKDB1108 Other Parts Discussed in Thread: LMKDB1102 , CDCE6214-Q1 , , LMK3H0102 Hi Sirs
I am finding a clock generator which's behavior like LMK1102 for PCIE application。
Our processor have one pair differential clock output, and plan…
Part Number: LMKDB1120 Other Parts Discussed in Thread: LMKDB1113 , LMKDB1112 , LMKDB1108 , LMKDB1104 , LMKDB1102 Tool/software: Hi team,
For below buffer, which can support power down tolerant? PDT stands for power down tolerance, which is usually…
Part Number: LMK6H Other Parts Discussed in Thread: LMKDB1108 Tool/software: Hello,
For an HCSL output, what differential output impedance should I set my traces to, 85 ohms or 100 ohms?
Best regards,
Zach Kimble
Part Number: CDCDB800 Other Parts Discussed in Thread: DS320PR1601 , LMKDB1108 Tool/software: Hi,
We are using CDCDB800 clock buffer along with DS320PR1601, in the said clock buffer's datasheet it is mentioned that default termination is 85ohm.
…
Part Number: LMKDB1102 Other Parts Discussed in Thread: LMKDB1202 , LMKDB1204 , LMKDB1104 , LMKDB1108 , LMKDB1120 Tool/software: Hello!
I am looking at the LMKDB12xx and LMKDB11xx family (they share a datasheet), and I am confused about the default…
Lik,
The LMKDB family of buffers is our latest and recommended solution for PCIe applications. The LMKDB1108 (8-output) and LMKDB1104 (4-output) are available for sampling now and meet all of your requirements. If your "clock generator" is only generating…