Thanks.
What will be feeding the input to this ADC EVM? What will the output of the DAC be connected to?
-> The output of D/A EVM is equal to specification of above referenced picture. The output swing as referenced single-ended is maximum 3.5V & minimum…
Other Parts Discussed in Thread: LMP8350 I am currently designing with LMP8350. I have encountered an offset at the input that I would like to null. What is the appropriate way to do this? Is there an alternate fully differential amplifier with similar…
Hi Idan,
Sorry the delay in reply. If you are planning to swing 10Vpp(diff) at the FDA output with ~1kHz, then either the THS4131 or LMP8350 could be used for your application. Both the devices operated on +/-5V supplies should be able to drive the 70…
Other Parts Discussed in Thread: LM2776 , LMP8350 Hi I am running 4 lmp8350 at +-5V from a 5V supply and -5V from the lm2776. One minute it is working appropriately, the next I am getting positive voltage from the negative output. It is either 1.8V or 0…
Other Parts Discussed in Thread: ADS1256 , LMP8350 , THS4531 Hi,
I'm interfacing a pressure sensor, with a 0-5v signal, to an ADS1256. What I'm looking for is a FDA that can turn sensors 0-5v signal in to a differential signal of +-2.5v with a zero…