Part Number: LMP8481 I'm using the LMP8481-H and want to add transient robustness circuitry. Does the max differential voltage of 667 mV (data sheet paragraph 9.1.1) also apply to the -H version? The -H has a Vsense max of 0.133 mV and I want to verify…
Other Parts Discussed in Thread: LMP8481 , DRV8881 , INA240
I'm using the LMP8481 to measure the current of a PWM servo system (driven by DRV8881)
The supply voltage to the circuit is between 20V to 35 VDC
There's an ambiguous note at the data sheet…
Other Parts Discussed in Thread: LMP8481 My customer is interested in using the LPM8481 in the WSON package. However, the datasheet only has part numbers listed for the VSSOP package. Is the LMP8481 available in the WSON package? If it is, can you please…
Hi Jacob;
Thanks for your reply,After testing, we found that there was a problem with the sampling circuit, and we used the LMP8481 to detect the high and low side currents of the 8770, but we ignored that the low-side current exceeded the rated value…
Part Number: LMP8645 Other Parts Discussed in Thread: LMP8481 , , INA240 Hello,
I’m looking at using the LMP8645/8640, but it lacks the reference input of the LMP8481.
Is there a similar part that has a reference voltage input? This would allow us…
Other Parts Discussed in Thread: LMP8481 Deer experts,
my question is about the supply voltages: can i set the ground level to -5V and the vcc level to +5V?
the supply voltage range is from 4.5V to 76V. so with my setting it would be 10V or?
i'm a little…
Part Number: INA169 Other Parts Discussed in Thread: LMP8480 , , INA170 , LMP8481 , LMP8640HV , INA240 Hello Support,
I am investigating possible current sense solutions in our application. The input voltage is battery powered Vin: 10V ~ 40V and the continuous…