Part Number: LMP90080-Q1 Other Parts Discussed in Thread: ADS114S08
Hello,
I was wondering, if I can integrate 3 wire measurement and 2 wire measurement on the same ADC ( P/N mentioned above) . Yes the ADC can handle up to 4 differential channels…
Part Number: LMP90080-Q1 Greetings,
Analog applied voltage, Va for LMP90080-Q1 specified as 4.75 - 5.5V.
Can it operate properly if 3.3V will aply to analog, Va?
Thank you,
Gadi Fishel
.
Hi Bryan,
I have not dealt with ADC chip having an option of external clock. I am in a dilemma whether to use the internal clock of adc itself or get a resonator. I heard internal clock are unstable. Do you have some insights on this?
FYI :I already…
Part Number: ADS124S08 Other Parts Discussed in Thread: ADS1120-Q1 , LMP90080-Q1 , ADS1148-Q1 Hi TI team,
I have 2 questions:
What is the maximum number of 4-wire RTDs that can be interfaced with this device?
What is the estimated layout area…
Hi Bharati,
The recommended operating conditions of the ADS1115 specify the maximum operating temperature at 125 °C. While the absolute maximum junction temperature is 150°C functional performance, accuracy and long term performance is not guaranteed…
Part Number: LMP90080-Q1 Other Parts Discussed in Thread: LMP90080 , ADS124S08 , ADS1248 , LMP90100 Hi team
can I get your reply ?
[1] I need to calculate TUE.
For worst TUE after calibration, I used INL = 1LSB, Offset = 15uV, Offset drift = 100nV…
Part Number: LMP90100 Other Parts Discussed in Thread: LMP90099 , LMP90098 , LMP90097 , LMP90080 , LMP90079 , LMP90078 , LMP90077 , LMP90080-Q1 Tool/software: Hi,
What is the protocol to read register data on my LMP90100?
Part Number: LMP90100 Other Parts Discussed in Thread: LMP90099 , LMP90098 , LMP90097 , LMP90080 , LMP90079 , LMP90078 , LMP90077 , LMP90080-Q1 Tool/software: Hi,
I'm enabling the CRC function in my LMP90100, but I'm only reading zeroes when I read…
This information is relevant to the entire family of devices, which includes:
LMP90100
LMP90099
LMP90098
LMP90097
LMP90080
LMP90079
LMP90078
LMP90077
LMP90080-Q1
Best Regards,
Angel
Part Number: ADS114S08 Other Parts Discussed in Thread: ADS1120-Q1 , ADS1148-Q1 , ADS1261-Q1 , ADS1018-Q1 , LMP90080-Q1
Tool/software:
Hi, I need to know if this ADC ADS114S0x Low-Power, Low-Noise, Highly Integrated, 6- and 12-Channel, 4-kSPS, 16…