Part Number: LMP92001 Hi E2E,
Good day.
The LMP92001 has an analog voltage output, is there a way that to read the output in digital using the I2C lines? Thank you in advance for the help.
Regards, Carlo
Part Number: LMP92001 Hi Sirs, As title, do we need external bypass capacitors on AFRE and DREF pins when internal reference was used? Can we leave them open? Thank you and Best regards, Wayne Chen 08/18/2020
Part Number: LMP92001 I am interested in your A/D, D/A ICs and have started to look at the different options that I have !
Currently I reviewed the TI LMP92001 and have a couple of questions :-
1. Is correct that this chip has a A/D sample rate of approx…
Hello TI,
1. Can you program the 12 Programmable Analog Voltage Outputs on a single I2C write or do you have to perform 12 seperate writes? Note each channel would have a seperate voltage value.
2. Can you set the device to continuously read each ADC input…
Other Parts Discussed in Thread: LMP92001 Hello everybody.
This is my first post in the forum and I would like to ask a question related with the data converter LMP92001. I would like to use this IC in my new design but I found one problem. When I switch…
Do you mean that the unity gain buffer is not required for the REF5020 and that readings I am getting are to be expected? I am trying to put all the components into one board i.e., 4 nos. LMP91000, 1 no. REF5020 and a 16 channels sigma delta or SAR ADC…
Kuan,
We don't have a single device that will fit all of your requirements so you might have to use more than one device. Here is the list. It looks like you might want to consider these: LM96194,LM94,LM93,LM96000.
HW_Fan_Parametric Search.xlsx
-…