Part Number: LMP92066 Other Parts Discussed in Thread: USB2ANY , I am using LMP92066 to generate gate voltages to an LDMOS device. The USB2ANY interface is also purchased to access the I2C ports of the IC. While installing the software the following error…
Part Number: LMP92066 We are using LMP92066 to feed gate voltages to NXP A3M35TL039 as per the reference from RAPIDRF-35TL039. One of the gate voltages is 5.7V. But the maximum possible voltage from LMP2066 is 5V. Please let us know how to generate 5.7V…
Part Number: LMP92066 Hi team,
I see that the Max EEPROM write cycles is specified as 100 Max. Is this correct? Customer's typical EEPROMS are specified for many more writes than this. Is that supposed to say 100K MAX?
Part Number: LMP92066 Hello. During evaluation of this device in my modules I continue to see the negative supply rail run away with excessive current and devices getting damaged, My eval boards have the VIO at 3.3V, VDD at +5V and VSSB at -5V. I have…
Part Number: LMP92066 As we know, LMP92066 is having internal switches to make the Bias voltages to 0V for the event of TDD.
we would like to have the provision of Having DAC and FETDRV pins functionality
As per the schematics, If we are using the FETDRVX…
Part Number: LMP92066 Hi Team, In our new project(in design stage), we are using DA GATE Driver from TI. The above mentioned schematic file is attached with this mail for your reference. So we request you to review it and provide your feedback. VVDN_TI_DA_DRIVER2…
Part Number: LMP92066 Hello. I have been using the LMP92066 in a few IRAD programs and now hopefully in production hardware. In two boards the -5V pin has shorted (1.7 ohms) and the devices are drawing excessive DC current. Those devices are now damaged…
Part Number: LMP92066 H team ,
We are measuring a internal teorature sensor of LMP92066 IC , we are getting below outputs :-
TEMPM = 1 TEMPL = EC TEMPM = 1 TEMPL = F7 TEMPM = 1 TEMPL = D9
So how we can convert into a dcimal temperature value…
Part Number: LMP92066
As shown in below image, There is a specified temperature range of -25 to 120 degC and an operating temperature as -40 to 125 degC. We need a lower temperature range of till -40degC so just wanted to check on this spec.
Part Number: LMP92066
Hi team,
I need to know the maximum junction temperature for the LMP92066PWPR . Also do you have a thermal model?
Thank you,
Vineeth S