Part Number: LMP92066
Hi team,
I need to know the maximum junction temperature for the LMP92066PWPR . Also do you have a thermal model?
Thank you,
Vineeth S
Part Number: LMP92066 Hi team ,
We are using LMP92066 DAC , In these we are able to get internal temperature sensor output . but how we can give the temp output to LUT ( look up table ) ? how to calculate LUT using 12 bit temp output ?
Part Number: LMP92066 What is the largest capacitance that I can place on the DACx pin? The datasheet says "the output buffer is designed to drive large capacitive loads, as high as 10uF".
What if I need to have 100uF capacitance in order to…
Part Number: LMP92066 Hi ,
LMP92066 is a dual DAC , So for DAC1 we want to keep constant output voltage , even though temperature is changing.
but in our case output voltage is changing w.r.t temperature change . so how we can keep output voltage c…
Part Number: LMP92066 Hi team,
On our DS, LMP92066 Power Supply line filtering/bulk capacitance recommends a 10 to 47 uF electrolytic cap on the VDD node, using a 10 uF tantalum cap on the EVM. However, there’s currently a shortage of tantalum caps, with…
Part Number: LMP92066 Hi
I use LMP92066 in my design. Now i have some question. Please help deal with it. Thanks!
1. I can use it for LDMOS without EEPROM. Now i want to use it to driver GaN. It can't work well. Schematic diagram as below.
2.Disconnect…
Part Number: LMP92066 Hi Team, We are using LMP92066_DAC, in these, we are able to get internal temperature sensor output (12 bit). but from the software side how to fill LUT 0 and LUT 1 (lookup tables) using temp output? what is the calculation for these…
Part Number: LMP92066 Other Parts Discussed in Thread: USB2ANY , There are two LMP92066 in our project (using IIC address to distinguish), we hope to complete the control of LMP92066 with a programmable interface controller. Do you have interface adapters…
Part Number: LMP92066 Hello, I am interested in the data retention period for the LMP92066 as it relates to the EEPROM. My application has a shelf life of 10 years with exposures to -54 to +95°C, non operating.