Part Number: LMP92066EVM Other Parts Discussed in Thread: LMP92066 , AMC7832 I am an RF engineer using LMP92066 EVM to bias LDMOS and Gan Power amplifiers (PA). I like to use it to drive an hybrid PA composed of one stage LDMOS and a second stage Gan, meaning…
Part Number: LMP92066 Hello, I would like to ask about the potential failure mechanism in the LMP92066 during 125°C operation or also in the event the temperature of 125°C is exceeded (estimate of 135°C)
Would this device have graceful degradation…
Hi Suddha,
The AMC7836 is a SPI slave, so it would still require a controller to program the device and extract the programming values from the non-volatile memory.
Could you consider a device like the LMP92066? This device features fewer channels but…
Part Number: LMP92066 Hi,
I am using LDMOS power amplifier and for that the gate voltage giving through the FETDRV and I am not using DAC output. So I am grounding DAC with 10uf.In this case how the connection of DRVEN should be both in HW side and SW…
Part Number: AFE20408 Other Parts Discussed in Thread: LMP92066 , LM27761 Tool/software: Hi,
We are using AFE20408 for biasing Power Amplifiers in my design (1 LDMOS, 2 GAN). I have two voltage sources +5.5v, +48v and -5v is required for GAN bias. Can…
Part Number: LMP92066 Hello,
We're having a few questions regarding LMP92066
Will IBIS model of LMP92066 produce accurate transient simulation results with any arbitrary load condition (capacitors and resistors)? I read that IBIS model is produced…
Part Number: LMP92066 Hi,
so far we've been working with LMP92066 device version A0 (marking 79AXN7U) which works just fine with excellent accuracy. Now we got a new batch of boards where the device version as read back in register 1F is A1 (device…
Part Number: LMP92066 Hello team,
please confirm that after programming the LMP92066 can be used without any uC in the final HW design.
As SDA and SCL will not be used how should they be connected, please?
Thanks and Best Regards,
Hans
Part Number: LMP92066
Hello support team,
I have a question regarding thermal pad of LMP92066.
Our customer wants to know the height value of the thermal pad . On page 62 of the datasheet, there is a package drawing of the PWP0016A. However, there is no…
Part Number: LMP92066EVM How do I change the "GaN Mode" from zero to one in the data path control interface. This question is mainly because I would like to know how to add negative voltages because there doesn't seem to be an obvious way.…