Part Number: LMQ64480-Q1 Tool/software: Hi Team, Can you please help me in schematic review above buck for customer
The requirement is to step down from 24V to 12V with an output current of up to 4A (including margin). PFB link for the schematics and…
Part Number: LMQ64480-Q1 Tool/software: I have a question about the internal structure of the LMQ64480QRXARQ1. Regarding the Lead Frame in the Material Contents Data, it is described as "Copper" + "Epoxy." Is this component a "MIS structure" component…
Part Number: LMQ64480-Q1
Tool/software:
Hello,
I'm looking for a DC/DC converter that's able to generate a dual output 5V/12V and I've found the reference LMQ64480-Q1.
With the help of the datasheet and the LM(Q)64480_A0_A2_Quickstart_Tool_REVA2…
Part Number: LMQ64480-Q1 Tool/software: Hello,
I have two questions about the LMQ64480QRXARQ1. www.ti.com/.../lmq64480-q1.pdf
Q1. The datasheet did not include the Package dimension diagram. Please provide the document 'MECHANICAL DATA'. Q2. The datasheet…
Other Parts Discussed in Thread: LMQ64480-Q1 Hi sir , please suggest part for
Dual output buck power supply , Vin nominal =15V, Vmin =12V, Vin max =16V, Vout 5V@3A and Vout 3.3 @2A, automotive grade
Other Parts Discussed in Thread: LMQ64480-Q1 , LMR14050 , TPS7A53B Hi Expert,
Could you recommend a buck solution with auto spec? thanks!
Input:12V(typ) 36V(max)
Output:0.8V/ 0.9V
Current: 3A
Far