Part Number: LMQ644A2-Q1 Hi,
I changed original simulation file for dual output configuration. However, simulation is not working properly. I set the output voltage to 1.3V but result's about 5v. Also there is unexpected ripple level on output.
I have…
Part Number: LMQ644A2-Q1 For LMQ644A2-Q1 part required input capacitor, Output capacitor and inductor selection guide for Adjustable output configuration. So, please provide some guidance.
Thanks,
Jignesh Karena
Part Number: LMQ644A2-Q1 Other Parts Discussed in Thread: LM61495-Q1 , , LM25149-Q1 Hello experts,
Our customer need to utilize a Buck converter to deliver 10A current at 5V under 105℃ ambient temperature in their ZCU project.
So they wonder if we did the…
Part Number: LM64460-Q1 Other Parts Discussed in Thread: LMQ644A2-Q1 Tool/software: Hello everyone,
I have designed a schematic using LM64460APPQRYFRQ1 for generating 1.5V/6A as output with an 18V DC input. Please find the attached schematic and kindly…
Hi Yoni,
I do not have a particular schematic for the LM70880-Q1 as the datasheet is still being worked on (a limited version is online) but you can look at the LMQ644A2-Q1 datasheet on page 24 to get an idea how two LM70880-Q1 will meet your design criteria…
Hi Edward,
I don't believe the input impedance is measured with this part nor is the logical relationship with MODE/SYNC and voltage at SW, but I can test this.
However, my advice is that siphoning the SW signal for this device is not tested and may…
Hello Far,
Please see below the device parameter search I did to meet your application:
Does your application need 0.8V or 5V? The parametric search is limited by the low VOUT of 0.8V since most of the current automotive grade converter internal feedback…