Part Number: LMQ66430-Q1 Other Parts Discussed in Thread: LMQ66430 , LMQ66420 Hi Expert,
Could you help to review the schematic for LMQ66430-Q1?
1.LMQ66430
輸入電壓Vin 12V
輸出電壓Vout 3.6V
Choke 2.2uH (Isat 5A)
power budget 2A
2.LMQ66430
輸入電壓 Vin 12V
輸出電壓 Vo…
Part Number: LMQ66430-Q1 Hello expert,
I'm wondering how much performance DRSS outperforms PRSS in the high frequency band(30MHz - 108MHz)
Could you please let me know?
Thank you.
Part Number: LMQ66430-Q1 Hello expert,
I found that LMQ66430-Q1 has integrated bypass capacitor, so it can reduce EMI.
But in datasheet, it seems it still use bypass capacitor
And even there are input capacitor selection guides.
How can I understand…
Part Number: LMQ66430 Other Parts Discussed in Thread: LMR54406 , LMQ66410
Hello Team
I'd like to concfirm validity of inductor selection design.
Our circuit requirement
Vin : 19V
Vout : 5.15V
Iout : 150mA (max)
I calculated inductor inductance constant…
Part Number: LMQ66430-Q1 Hello,
The datasheet of the LMQ66430-Q1 states that
Open-drain power-good flag output. Connect to suitable voltage supply through a current limiting resistor. High = power OK, low = power bad. This pin goes low when EN = low…
Part Number: LMQ66430-Q1 Other Parts Discussed in Thread: LMQ66430 , Hello,
Is the PSpice model of LMQ66430 only supported by PSpice for TI?
I can't run the simulation with SIMetrix environment even though I succeed to import the library to SIMetrix.…
Part Number: LMQ66430-Q1 Hello Team,
LMQ66430-Q1 data sheet in the Orderable Part Number column, I could see LMQ66430MC3RXBRQ1 is used for fixed and Adjustable version can you explain me how this IC can understand is it fixed or adjustable version from the…
Part Number: LMQ66410 Other Parts Discussed in Thread: LM61480 , LM61495 , LM62460 , LMQ66420 , , LMQ66430
Hi support team,
Are the differences between LMQ66410, LMQ66420 and LMQ66430 the same as the differences between LM62460, LM61480 and LM61495?
・Current…
Part Number: LMQ66430 Hello,
WebBench recommends RFBT = 4.99 kΩ and RFBB = 10 kΩ for an output voltage of 1.5 V on the LMQ66430.
Equation 5 of the data sheet says: 5 kΩ ≤ RFBT || RFBB ≤ 10 kΩ.
The parallel combination of…