Hello,
For the +12V to +10V application, you may be interested in the recently released converter (integrated FETs) LMQ66430-Q1 https://www.ti.com/lit/ds/symlink/lmq66430-q1.pdf .
For the +12V to -12V application, you would need to convert a buck…
Hello,
As far as I'm aware there is not a plan to stop production of the LM53635MQRNLTQ1.
In terms of an alternate device, LM63635-Q1, and LMQ66430-Q1 both have the same functionality with a different pinout. LM63635-Q1 36V, 3.5A converter while the…
Part Number: LMQ66420-Q1 Other Parts Discussed in Thread: LMQ66420 , LMQ66430 Hi Expert,
Could you help to review the schematic for LMQ66420-Q1?
1.LMQ66420
輸入電壓Vin 12V
輸出電壓Vout 1.8V
Choke 2.2uH(Isat 5A)
power budget 1.5A
2.LMQ66420
輸入電壓Vin…
Part Number: LM62440-Q1 Other Parts Discussed in Thread: LMQ66430 , Hi team,
I asked tEN of LMQ66430 before in E2E and found it also includes VCC start up time.
I measured from EN rising edge to the device start switching and the result was 2ms while…
Part Number: LM64440-Q1 Other Parts Discussed in Thread: LMQ66430 , LMR43620-Q1 Tool/software: In terms of efficiency there is a pretty large difference between the quick start spreadsheet and the WebBench version , it is very obvious at light load. …
Part Number: LMQ66430 Dear Support,
I just completed a design with LMQ66420R5RXBR , and turns out couldn't find it on the market. looking for alternative here is the device naming nomenclature from the data sheet
LM X 664 X 0 X X X RXBX – Q1.
…
Part Number: LMQ66410-Q1 Other Parts Discussed in Thread: LMQ66430 Hello Dear TI Team,
Regarding the LMQ66410-Q1 device, according to its Data Sheet, SNVSC78B – FEBRUARY 2022 – REVISED MAY 2023, 5 Device Comparison Table on Page 3,
there is a device…
Part Number: LMQ66430 Hi Community,
upon downloading the LMQ66430 simualtion file I noticed several issues:
LMQ66430-Q1_TRANS_ENCRYPTED.LIB has an absolute path definition!
RDSLS and RDSHS are global parameters in encypted part of the model and…