Part Number: LMR10510 Other Parts Discussed in Thread: LM2830 Hi
What is the main differences of LMR10510 and L M2830. Upon checking their datasheet electrical parameters are the same. What is the advantages of the two? The only difference found in the comparison…
Part Number: LMR10510 Hi team,
My customer asked me what the symbol "D" indicates in the formula on page 15 of the data sheet.
9.2.1.5 Catch Diode
ID1 = IOUT x (1-D)
Regards,
Part Number: LMR10510 Hi,
According to the datasheet , for the LMR10510X 3V3 1A output, R1 needs to have a value of 45K3 and R2 needs to have a value of 100K (see figure 9.2.3.2, page 18). However, according to chapter 9.2.1.6 (page 15), the resistor values…
Part Number: LMR10510 Stability issue reported by a TI Customer-
We came across a stability issue of switcher regulator LMR10510XMF/NOPB. As shown in the schematic below, C81P CAP 10nF was recommended by TI for Vout = 1.8V for LMR10510XMF for stability…
My customer asks:
We have a load at 3v3 that takes from about 100mA to about 400mA, depending on what’s turned on.
We’re trying to step down from USB input, so a nominal 5v0, but ranging from 4v5 to 5v5.
Trying it out at the low end of the…
Other Parts Discussed in Thread: LMR10510 Hello everyone . I need ZETA DC-DC from 3,7 V to 6.4V at a current of 50mA.
LMR10510 suitable for this? According to 7V datasheets will not damage the chip , I also need 6.4 V.
Other Parts Discussed in Thread: LMR10510 Hi Team,
Customer wanting to enable LMR10510/10515 with output of 1.8V LDO, but is concerned about zero margin in the design. In the datasheet there are no diagrams regarding the dependancy of this signal to any…
Hi Vamsi,
We found the issue, that 1.2v voltage regulator LMR10510 couldn't deliver enough current, maybe there is a design issue. Thanks for your help.
Cindy
Part Number: TMS320F28375S Other Parts Discussed in Thread: LMR10510 , LM43602 , UNIFLASH , LM2830 Hello.
I have a PCB with a TMS320F28375S. The situation is, that code execution in the controller stucks (controller hangs up?), when the different controller…