Part Number: LMR14006 Hi,
my customer has make buck circuit with LMR14006 for 5V output, input range is 9-32V.
Diodes is SS16, datasheet link is as below:
https://www.panjit.com.tw/upload/datasheet/SS12_SERIES.pdf
They have make 2000pcs board…
Part Number: LMR14006 Dear Sir/Madam,
We are preparing a new product development and planning to use your Step-Down Regulator LMR14006Y.
Attached a capture of the schematic, this is based on Webench tool. Output voltage has to be 9.62V. Load will…
Part Number: LMR14006 Hi, I downloaded both type of PSpice files from the website: https://www.ti.com/product/LMR14006 and extracted them, saved to a folder called spicelib. When I was creating the new macro on TINA, it gave me different errors. Please…
Part Number: LMR14006 Hi,
We realized that in the LMR14006 datasheet all Electrical Characteristics stated only for TA= 25°C because there is the statement "VIN= /SHDN= 12V,TA= 25°C, unless otherwise specified." at top of Electrical Characteristics…
Part Number: LMR14006 Dear all,
we are checking a design done by one of our contract manufactures. It uses a LMR14006XDDC.
The circuit is used in an environment with a large range of input voltages from 12V to 40V.
The output voltage is 3.3V at…
Part Number: LMR14006 Hello,
LMR14006Y min on time is 95ns. swtiching frequency is 2415kHz is tougher condition I think. 2415kHz period is 414ns.
Duty will be around 24% = 95ns/414ns.
When Vout is 12V desired, around 50V = 12/0.24 is max possible…
Part Number: LMR14006 kindly let us know the working capability of buck converter IC LMR16004 when ramp down and ramp up voltage is applied continuously to IC.
This ripple voltage will be controlled by externally components. Ripple timing is based on…
Part Number: LMR14006 Hi team,
Could you give me advise on how to answer the following customer question? The customer has seen schematic with a capacitor is connected to the feedback pin, but they're not sure how to select it and its requirement. Also…
Part Number: LMR14006 Dear all,
one of our contract manufacturers delivered a design with a LMR14006XDDC.
We would like to calculate the output drift of the supply voltage over temperature, but the values are not specified in the datasheet.
The…
Hi Nagapooshnam,
CST is not a tool that we support for our models. Since the unencrypted model for this device is freely available on the product folder for LMR14006, you are free to share that with the CST tool vendor who can help debug why this is…