Hi Nagapooshnam,
CST is not a tool that we support for our models. Since the unencrypted model for this device is freely available on the product folder for LMR14006, you are free to share that with the CST tool vendor who can help debug why this is…
Part Number: LMR14006 Other Parts Discussed in Thread: TPS54060 Hi,
Has anyone tried to use the LMR14006 as a inverting converter? From my understanding, the LMR14006 could be used as the TPS54060 to get an negative output. I want to design a simple…
Part Number: LMR14006 Tool/software: WEBENCH® Design Tools Hi team,
Could you give me comments on the following customer questions?
<Customer question>
For the outputs from WEBENCH like schematic and BOM, is it verified by lab bench or calculation…
Part Number: LMR14006 Hi
Our customer has following requirement.
Device : 14006X (Fsw=1.1MHz)
Vin: 13V-30V
Vout:12V
Iout:0.1A
We are considering following way to select inductance. Could you please review it?
1.
Supposing Iout=0…
Part Number: LMR14006 Hi,
In order to get a slower Vout startup than the fixed rate (not delayed, but lowering dV/dT) I wonder if the top resistor R1 could be shunted by a PFET and a capacitor such that the PFET is On for 100ms while the capacitor gets…
Part Number: LMR14006 Is LMR14006YDDCT in production? Distributors have zero. Either this is at start of life or end of life, I need to know which. When will stocks be restored?
Part Number: LMR14006 Other Parts Discussed in Thread: TPS61072 Hi,
I have two power sources that I need to combine, one from a step down converter (LMR14006) and the second from a step up converter (TPS61072). I can do this by switching the outputs…