Part Number: LMR14010AEVM Other Parts Discussed in Thread: LMR14010A Hi
I have designed LMR14010 based on LMR14010AEVM and the output voltage is correct but the problem is inductor is very hot.
Also, do you have the Gerber file for LMR14010AEVM…
Part Number: LMR14010AEVM Why is this EVM only rated for 9-18V input (less than half device operating range)? Are there any modification needed to operate to higher voltages?
Part Number: LMR14010AEVM The datasheet says the part can be stored down to -55C, but only operates down to -0C.
Is there a similar device that can operate down to -55C?
Part Number: LMR14010A
Dear Sir/Madam,
I wish to evaluate the LMR14010A but i cannot find LMR14010AEVM in the TI store. It is still available?
i only can find the link here
Best regards, kpk
Part Number: LMR14010A Other Parts Discussed in Thread: LMR54410 , LM5158 Hi all,
I've been testing LMR14010AEVM Evaluation board and I have a trouble. I've modified PCB for VIN=35V, Vout=27V/750mA, Cout = 4.7uF x2 + 100nF
With Resistive Load is working…
Part Number: LMR14010A Other Parts Discussed in Thread: TPS560430 Hello support team,
My customer would like to know a threshold current to exit the ECO-mode from no load. They are using LMR14010AEVM with Vin=24V and Vout=5V.
Thanks and regards, …