Part Number: LMR14030-Q1 Other Parts Discussed in Thread: LMR14030 , LM5149 I would like to use LMR14030SQDPRTQ1 for making +12V, 2A power supply.
I have one requirement in the circuit that if 12V input is given to IC, the output should be 12V. Is this…
Part Number: LMR14030-Q1 Other Parts Discussed in Thread: LM63635-Q1 , LMR14030 Hi, Can you confirm whether LMR14030-Q1 is equivalent to ASL B rated IC. If not, could you please explain why not? Could you recommend and ASIL rated IC with the same/EMI…
Part Number: LMR14030 Hi Team,
My customer got an issue using two LMR14030 with Sync pin in parallel.
It's look like that one of the device is instable.
They used the draft from the datasheet FIG 17 left schematic not knowing if their input clcok…
Part Number: LMR14030-Q1 Hi team,
Is there any concern if I use 0.22uF as Cboot of LMR14030-Q1 while 0.1uF is recommended?
Could you please advise the maximum value I could use for Cboot?
regards,
Part Number: LMR14030 Hello Team,
I am going through Application report SLUA844B.
I have few queries, on the topic "thermal characterization parameter" discussed. I wanted to raise a question on this Report, but the forum is asking for a part number…
Part Number: LMR14030LMR14030 SS QDDARQ1 has spread spectrum, if I use external PWM input RT pin, is it can replaced by LMR14030 S QDDARQ1(no spread spectrum), or replaced by LMR140 50S QDDARQ1(output 5 A current, no spread spectrum)?
Part Number: LMR14030 Hi TI expert
I set output voltage is 12.8V, when input voltage is higher than 12.8V, it can works well.
But when input voltage set lower than 12.8V, the Inductive sounds noise.
Here is my schematic. Please help to check…
Part Number: LMR14030-Q1 Am I correct in thinking that when Webench reports a negative gain margin, it actually means the gain is negative at the phase crossover and therefore (GM (dB) = 0 - G(dB) @ phase crossover) the system has a positive gain margin…
Part Number: LMR14030-Q1 Hi Team,
We know from DS that IQ=40uA(typ) when Tj=25C.
Customer consulted us when Tj=85C, roughly, what value will IQ become?
Kindly help to advise. Thanks.
Best regards,
Terry
Part Number: LMR14030-Q1 Other Parts Discussed in Thread: LMR14050 Hi, TI Support Team
I am trying to configure USB CAHRGER as below BLOCK.
Previously, two LMR14030-Q1 products were used as INPUT of USB CHARGER IC, but to reduce to one, the block…