Part Number: LMR14030-Q1
Dear,
We are using TI LMR14030-Q1 package HSOIC-8 . Pin No 6 soft start we connected 2.2nF, SMD ceramic capacitor, Recommended capacitor greater than 8.2nF. . can we change capacitor value to 10nF
Best regards,
Hitainder…
Part Number: LMR14030 Hi,
Recently I built a BUCK(from 24v to 12v) using LMR14030 with the schematic as below, but it doesn’t work well. We observe some very low freq noise in Vin, could you give us some suggestions?
Thanks.
BR
Mason
Part Number: LMR14030 Hi Experts,
We have a few questions regarding the LMR14030.
It's perfect for our customer needs of converting 24 V to 5, 10, and 15 V. But they need also an inversion to -15 V. Are there possible circuit solutions to generate…
Part Number: LMR14030 Hi support team.
I have a question about below.
Could you please tell me "free-air temperatuire"?
LMR14030 does not have specified operation ambient temperature.
Best Regards,
HIga
Part Number: LMR14030-Q1 Other Parts Discussed in Thread: LMR14030 Please help to provide calculation or Formula for minimum startup voltage.
for example, the output voltage is set to 3.3V or 5V, what is the input voltage will be able to gerenate 3…
Part Number: LMR14030-Q1 Other Parts Discussed in Thread: TPS54388C-Q1 , LMR14030
Hi Expert,
Our customer use LMR34010 and TPS54388C-Q1 in the same design. Since there is no MCU in system, they would like to connect PG form LMR14030 to…
Part Number: LMR14030-Q1 I downloaded the avgerage model of LMR14030S_Q1 from TI offical website, and want to do simulation with Pspice.
I want to know what's purpose of adding Linj , Cinj and V6?
Part Number: LMR14030-Q1
Hi Team, seeking your assistance.
Encountering a large spike immediately upon plugging in Vin, long before the LMR14030-Q1 has started switching.
Webench project
https://webench.ti.com/appinfo/webench/scripts/SDP.cgi?ID…
Part Number: LMR14030 Hi team,
Customer met EMI fail @200MHz in their design at heavy load(seems fine at light load). They tried to change switching frequency but failure still same. Below is a schematic of their design and I dont have the layout on…