Part Number: LMR14050 Tool/software: Hi all
i have an issue with hysteresis on the LMR14050 chip
I want a turn on voltage of 12.5V and turn off voltage of 11V
i use Rent = 416k
Renb = 42k
The power supply turns on OK. But when reducing the input…
Part Number: LMR14050 Tool/software: Team-
Please find attached +12V to bipolar +/-15V output switcher based on the LMR14050.
I have this TINA simulation working, but since this uses internal compensation, could use some help to get the loop stable…
Part Number: LMR14050LMR14050 Switching Waveform as below,is this Subharmonic oscillations?
300mA load
1A load
I think LMR14050 have slope-compensation,and will not have Subharmonic oscillations,right?
Thanks!
Part Number: LMR14050 HI,
We are using LMR14050 IC in one of our design, we have given all the necessary EMI-Filter circuitry mentioned in the application note.
But still the CE102 graphs are behaving similar to one which is given in the application…
Part Number: LMR14050 Other Parts Discussed in Thread: LM5117 Hi, I've few questions about this schematic. I use the LMR14050 to charge 1S/2S/3S IO-LITH batteries by monitoring the charge current with a INA series current sense. *Is stable the buck converter…
Part Number: LMR14050-Q1 Tool/software: Hello, Team,
Our customer would like to know how to estimate the frequency will fold-back when the OCP is triggered. Is there a way to estimate how much Fsw will drop?
Device: LMR14050SQDPRRQ1
Best, M…
Part Number: LMR14050 My customer was using LMR14050 for the below application:
Vin=24V, Vout=12V/ 2A.
They found the voltage output showed some unexpected ripple/spike during the soft start, with full load startup.
The issue was found if using…
Part Number: LMR14050-Q1 Tool/software: Hi experts,
I'm KIM
I am working on a buck converter design using **LMR14050SQDDAR (non-spread spectrum)** to charge a **3-cell Li-ion battery** with these target specs:
- **Input Voltage**: 30V (bench supply…
Part Number: LMR14050 Dears,
Customer use the LMR14050SDDAR with -10℃ and can not find the current vs temp data,could you pls kindly help to provide it?
Thanks