Part Number: LMR14206 Tool/software: Hello,
I have tested LMR14206XMK/NOPB this IC for surge protection, and i had applied 2KV to Live to Neutral, But IC did not sustained the surge, The circuit protection is in below attached image.
The previously…
Part Number: LMR14206 Hello All,
I am selecting LMR14206XMK/NOPB IC for my new design.
the design requires the CE qualification so according to that the device should sustain 2KV at input for Live to Neutral and vice versa, for 8/20 uS Surge current…
Part Number: LMR14206
Hi Team,
my customer has the following request:
We would like to replace the TPS560430XF with the LMR14206. So far this works, the only thing we miss is the behavior of the enable pin with the hysteresis: In the datasheet…
Part Number: LMR14206 Hello,
The SNVA856A AppNote deals with using buck DC-DC convertors in instead of inverting buck-boost (IBB), where negative voltage is needed.
Is this technique valid for all buck converters circuits ?
This technique suppose…
Part Number: LMR14206 Other Parts Discussed in Thread: LMR36006 Dear all,
can anyone help me with an EMC issue I am having with this regulator?
I am following the reference design and I have added an additional filter at the input, but the conducted…
Part Number: LMR14206 Hi,
the application report SNVA856A describes how to transform an ordinary buck regulator into an inverting configuration.
Is it possible to use the LMR14206 for such an application?
I want to generate around -15V from +15V…
Part Number: LMR14206 Other Parts Discussed in Thread: TPS62097 LMR14206 failures issue
We have a design 24v/12v input to 5 v rail typically 20mA, max 100 mA using a LMR14206.
The 5 V rails feeds a TPS62097 Step Down Converter for the 3.3 V rail…
Part Number: LMR14206
Hi Team,
The customer feedback the LMR14206 have some issue that is come from SW pin signal is not stable and let his output drop a little bit.
But when he change to older one datecode LMR14206(around one years ago) will…
Part Number: LMR14206 Other Parts Discussed in Thread: LMR14006 , Hello, We have replaced the LMR14006 with the LMR14206 for logistic issues.
The SHDN pin is floating in our PCB and, now, the new regulator does not work properly. In the datasheet of…