Part Number: LMR16006 Hello,
I would like to properly size a resistive network to control the turn‑on and turn‑off behavior of the LMR16006XDDCR based on the input supply voltage. For this purpose, I need the specific ON and OFF threshold values of…
Part Number: LMR16006 Hi,
What is the difference between LMR16006YDDCT and LMR16006YDDCTG4?
Please share the document which explains the difference.
Thank you.
Part Number: LMR16006Y-Q1 Other Parts Discussed in Thread: LM51551-Q1 , LM51551 , LMR16006 , TPS560430-Q1 , TPS560430 , LM5155 Hello TI team,
I’m Ali, an external HW engineer at Emotors, I am currently working on a power supply architecture using…
Part Number: LMR16006 Tool/software: Hello TI Team,
We are designing the following power supply circuit using IC: LMR16006YDDCR, however we found a discrepancy between the specs in the datasheet and the TI Webench simulation.
1. Design requirements…
Part Number: LMR16006 Tool/software: I am testing a buck converter evaluation board LMR16006EVM. This LMR16006 has an ECO mode which terminates switching when the load current is very low.
This is the schematic of LMR16006EVM.
The board is connected…
Part Number: LMR16006 Tool/software: Hello,
I have a 48V-7V DC-DC implementation using the LMR16006. After the initial transient, the datasheet specifies a -0.3V max from SW to GND. My understanding is that on the off cycle, the SW to GND voltage…
Part Number: LMR16006 Tool/software: Hi Ti,
I am now learning the block diagram of LMR16006, and I want to figure out what function do these blocks have.
For bootstrap regulator, I know it is used for C_boot charging, but I do not know what exactly…
Part Number: LMR16006
Hello,
I having trouble getting same value for output inductor value by using formula from LMR16006 datasheet. Please refer to 9.2.1 Custom Design procedure.
Parameters:
Input Voltage: 16V
Output Voltage: 5.0V
Output…
Part Number: LMR16006 Hello, I tried LMR16006 WeBench with the following settings. However, WeBench says “Design cannot be created!” What’s wrong?
I also tried other avaiable devices for WeBench, but with the same result.
Part Number: LMR16006 Tool/software:
Hi, friends
This is the block diagram of a BUCK switch converter LMR16006. I want to know what the SS means for the input of the error amplifier. I know the 0.765V is the reference of error amplifier, but what…