Part Number: LMR16006LMR16006 is a non-sync mode,when the buck regulator works in CCM , how to charge the Cboot cap?
-when the high-side MOS open, CBoot cap discharges,
when high-side MOS close, the inductor L1 current began to flow through the diode…
Part Number: LMR16006
Im experiencing periodically bumps in my 3.3V signal as shown in picture below.
These bumps are too big for me to accept for my design in application for 4-20mA loop signal.
Current through LM16006 fo rmy application is about…
Part Number: LMR16006 Dear team,
Customer use LMR16006, schematic as below, when BATT voltage>32V, LMR16006 failed when power on, vin=vout. When customer increase the output capacitor to 30uF, the fault will happen when BATT>40V. Customer must use 1uF…
Part Number: LMR16006 Is it possible to use LMR16006Y version to convert 24V to 3.3V with 0.4A current output? We see only X version in TI Webbench to convert to 3.3V. Please guide.
Part Number: LMR16006 Other Parts Discussed in Thread: LMR16010 , LMR36006 , I am using the LMR16006 with the output set to 6.5V. In my application is it possible for Vin to be less than 6.5V, and my desired behavior is for the LMR16006 to simply pass…
Part Number: LMR16006 Dear Team,
What is the difference between LMR16006 X DDC and LMR16006 Y DDC , I can’t see it in the data sheet.
Many Thanks,
Jimmy
Part Number: LMR16006 Other Parts Discussed in Thread: LMR36006 , LMR36006-Q1 Hi Team,
Our customer would like to confirm if he can drop-in replace a LMR16006XDDCR with a LMR16006YDDCR. The datasheet shows that the difference between the two devices…
Part Number: LMR16006 Hi Team,
I'm helping customer to check the difference btw LMR16006-q1 vs non-q1.
To my surprised, they have some differences besides AEC Q100. It's my first time seeing Q-grade has different spec.
Just want to confirm about…
Part Number: LMR16006 Other Parts Discussed in Thread: LMR16030 , Hello,
in our Design with LMR16006 and LMR16030 in a BLDC Controller almost all LMR16006 fails after some time of driving.
And sometimes the LMR16030 fails with broken case.
Both…