Part Number: LMR16006XEVM Other Parts Discussed in Thread: PSPICE-FOR-TI Tool/software: Hi, i am trying to run ltspice simulation with psice model of lmr16006x_transient as following: I imported every pin accordingly to the .lib file:
CB-->1 GND-->2…
Part Number: LMR16006XEVM Hi,
We want to change the output voltage from 5V to 3.6V on LMR16006XEVM. Please let me know how to change the voltage.
Thanks and best regards, M.HATTORI.
Part Number: LMR16006 The signals on the output are rather noisy and I would like to speak with someone or obtain additional information on reducing the noise levels (see oscilloscope captures below). The 2nd PNG file show the zoom for the oscillation…
Dhanraj,
I did not have any issues simulating the circuit in PSpice, however, I used the reference design (STARTUP) that is in the product folder. I also added a simple 1K resistor as a load for the output. Here is the circuit:
I am attaching the…
Part Number: LMR16006 We are designing in this regulator as per the reference design in LMR16006XEVM. C4 and C5 are large MLCC ceramic capacitors. Unfortunately these types of caps are high risk due to global supply chain shortages. Can we substitute…
Part Number: LMR16006 Hi
I want to confirm LMR16006 operation under following condition.
Vin:12.5V
Vout:12V
Iout:50mA
I obtained following waveform using LMR16006XEVM.
1. CH1:SW, CH2:VOUT
12Vout seems to be regulated.
Is the switching…
Hi David,
I verify it on LMR16006XEVM, Vout is default 5V, Vout can track Vin till Vin drop to 4.4V.
Low drop out and no load condition is worst case for Cboot refreshing, LMR16010 has smaller inductor to get higher current peak when Vin is close…
Part Number: LMR16006 I want to use lmr16006x to charge a bank of four 10.000uF capacitors. The capacitors are used for bridging power supply in case of power fail. The idea was to use the FB-Pin to set the final voltage and to use the internal peek current…
Hi Yang-san
Thank you for your support.
>As Akshay suggested, have you tried to reduce the switching frequency? You can send us the schematic and layout for review.
Not yet. We are trying to get the EVM of X version (LMR16006XEVM). You can refer…