Part Number: LMR16010 Tool/software: Hi
I haven't been able to locate the MS Excel file mentioned in this video, is it possible to attach it to this post?
Thanks
https://www.ti.com/video/3877721406001
www.ti.com/.../snva489c.pdf
SNVA755 uses…
Part Number: LMR16010 Tool/software: The circuit design closely follows the EVM, with the only modification being the feedback resistor values to set the output voltage to 3.3V. We are switching between two input power supplies, both supplying 33V. However…
Part Number: LMR16010 Tool/software: Hello, im trying to export my design through the CadSoft Eagle Option and after waiting for several minutes I receive an Export Failed message.
This is my design:
webench.ti.com/.../10
I tried with Chrome…
Part Number: LMR16010 Tool/software: Hi,
I tried simulating the circuit of LMR16010 on TI's webench and I altered the values to the calculated values based of the formulas of the datasheet. The Cout value calculated is about 5uF. I have changed the…
Part Number: LMR16010 Hello,
We have a problem with the radiated emission of our product. It exceeds the limits of the CE radiated emission testing. After a long search we didn’t find the source of the problem. So to verify that the problem is in…
Part Number: LMR16010 Other Parts Discussed in Thread: LMR38020 Hi,
May I ask for 30pcs samples for our new design purpose since there is no stock available in TI.com.
Besides, any other alternatives can be suggested?
Thanks,
Vito
Part Number: LMR16010
Hello expert,
I am doing an FMEA of the 5V regulator and wondering what the expected VOUT and effects are for the following cases. See simplified schematic and component values listed below.
Short CBoot
Open CBoot
Short…
Part Number: LMR16010 Hi Support team,
my customer encountered start up VOUT negative slew rate issue, the same thing also occurred in EVM while output have loading
following is measured result in EVM
VIN 50V VOUT 5V @ 0.15A operation frequency…
Part Number: LMR16010 I am looking for the best way to add a delay of about 10 seconds between when power is applied and when the LMR16010 is enabled. Adding a simple RC to the EN pin seems like an easy way to do it. However I think it may be even easier…
Part Number: LMR16010 Hi Team,
My customer wants to check if LMR16010 OVP function can work normally, is there any OVP test method that my customer can refer to?
Regards,