Part Number: LMR16010 Hello E2E,
We found double pulse at no load/light load.
Is it normal?
if yes, could you please explain the reason?
If not, how to improve it?
<Zoom-in>
<Zoom out>
<Schematic>
BR,
Jason
Part Number: LM5160A Other Parts Discussed in Thread: LMR16006 , LMR16010 , LM5160 Hi team,
whether the LM5160A and LMR16006, LMR16010 can support the 5~53V input, 3.3v output? We want to check the Dmax. Thanks.
Part Number: LMR16010 Hi,
I have some doubts about the startup waveform of LMR16010. (24V input & 12V output)
- Yellow: SW current
- Blue: Vds
- Pink: Input
- Green: Output
Question1: why there has 3 valleys?
Question2: why intermittent SW ON/OFF…
Part Number: LMR16010 ctm used other brand DCDC, with seems pin compatible but the power good pin is comp.
Can LMR16010 work with 2 cap and 1 resistor on the power good pin?
Thanks.
Part Number: LMR16010 Dear all
I check "Material content search", as the link : www.ti.com/.../search
1. I don't know what is the meaning of "Ext-Mfg" ?
2. Is there other Assembly site ? Could you share detailly to me ? …
Hi Arief,
Attached is a .pdf of the design layout. If you wish. I'd like a EVM to look at.
Send to:
Rapid-K Energy Solutions, LLC
2103 W Parkside Ln.
Suite 105
Phoenix, AZ 85027
2133.TI LMR16010 Design.pdf
Part Number: LMR16010 Tool/software: WEBENCH® Design Tools The input voltage is 42VDC and I want to get 15VDC / 1A output. But WEBENCH cannot output a solution on LMR16010. Is it a problem about WEBENCH? Who can tell me the input/output capacitor, inductor…
Part Number: LMR16010 1.For the Figure 8 Dropout Curve in the datasheet, I did not observe the turning point when Io=0.2A at Vin=5.2V. What is the reason that the dropout curve with Io=0.2A takes a lead to Io=0.05A at nearly Vin=5.2V?
2.For the Figure…
Part Number: LMR16010 We are using the LMR16010 in a circuit that provides closed-loop current control for a 0.5H, 60-ohm solenoid coil.
In this application, the LMR16010 GND pin is connected to -15V and its VIN is connected to +15V. Signal THP is connected…
Part Number: LMR16010 Tool/software: WEBENCH® Design Tools Design specs: 48V in / 24V out / 1A
Why are Rfbb and Rfbt not shown in 0402 packages?
The webench tool show values of:
620k (Rfbt with package 0603 ... 1206)
20k (Rfbb with package 0805 ... 2010…