Part Number: LMR16030 Hi Support Team,
We are currently working on a project using the LMR16030 and would appreciate your help with a schematic review.
Here are our key design parameters:
Input Voltage : 9-36V
Output Voltage : 5V
…
Part Number: LMR16030 The charging conversion circuit uses the LMR16030 from TI. The following is the design diagram. Could you please help check if there are any issues?Thks
Part Number: LMR16030 Hi Support Team,
We have a project using the LMR16030 (U1) with VIN = 12V , VOUT = 3.3V , and IOUT = 3A (max) . The attached files include the circuit design and PCB layout. Could you please help review them and let us know if…
Part Number: LMR16030 Other Parts Discussed in Thread: LM70840 , LMR38025 Hi, I’m having an issue with the power input to the LMR16030 at 58 V DC.
I’m using the LMR16030 to regulate an input voltage of up to 58 V down to 12 V. During lab tests, when…
Part Number: LMR16030
my dought was reguarding the pin SW suppose i want output voltage 12V. which is greater than 6.5V in which it is mentioned that BOOT to SW max so it that means that reguarly we see connecting BOOT pin to SW for 5V output which…
Part Number: LMR16030 Hi
At the moment of power on, there is a surge current of about 800mA at the input terminal, which cannot pass the certification. How to reduce it?
The schematic diagram and PCB of the customer are as follows. The power supply…
Part Number: LMR16030 Tool/software: Hi Team,
Create a BUCK power supply using LMR16030, with an input of DC 18~60V, output of 24V, and a current of 0.8~1.5A What should be paid attention to in circuit compensation? What is the output state when the…
Part Number: LMR16030 Tool/software: Dear expert,
Is it mandatory to connector the SS to a capacitor for LMR16030SDDAR or if it is not connected it will be seen
as a very small (pF) cap with the internal capacitor?
Thanks,
Andras Magyar
Part Number: LMR16030
Tool/software:
Hi All,
I have a question about the thermal information of LMR16030. Please tell me the measurement conditions. For example, a 4-layer board with a size of 100mm x 100mm,etc,,,
Best Regards, Ishiwata
Part Number: LMR16030 Tool/software: Hi All,
I have a question about the thermal information of LMR16030. Please tell me the measurement conditions. For example, a 4-layer board with a size of 100mm x 100mm
Best Regards, Ishiwata