Hi Ishiwata-san,
I responded to the other thread. let me close this one.
https://e2e.ti.com/support/power-management-group/power-management/f/power-management-forum/1397699/lmr16030-thermal-information
Thanks,
Richard
Hi Ishiwata-san,
Looks like this EVM didn't undergo the thermal simulation but instead it is based off the LMR16030 and LMR38020DDA test.
Thanks,
Richard
Part Number: LMR16030 Tool/software: I am having issues with a LMR16030S, the output is noisy even under no load, and then when load is applied (using a resistor) the voltage drops to ~600mV. The circuit is very noisy - both on the scope output and …
Part Number: LMR16030 I am using this regulator for a project, and the switching frequency is extremely low. The ripple is also terrible, although this is likely a symptom of the lower-than-expected switching frequency.
We get +4.7 V out, so it is regulating…
Part Number: LMR16030 Dears,
C ustomer found that the inductance affected the SW output waveform, which made the output abnormal. Does inductance affect the SW waveform? What is the cause
The first inductance is TDK SLF10165T-100M3R8-3PF, it make SW waveform…
Part Number: LMR16030 Dears,
After the bottom of the inductor is coated with plastic, the duty cycle of the SW output waveform decreases from 25% to 5%, resulting in heat;
The customer's power supply is used in a variety of products. In one product, the…
Part Number: LMR16030 Other Parts Discussed in Thread: TPS563210A Hello
i would like to use the LMR16030SDDAR and i have 2 questions about this part:
attached are my schematic and the datasheet...
my parameters are : input = 18-60V , output = 15V (3A…
The LM317KCS datasheet is TI part, C was a mistake. Anyway the LMR16030S steady state Spice model peak voltage exceeds 27v out when zoomed in at the end of the graph. The Webench Pspice FB loop sense resistors are to maintain roughly 23.99v output for…