Part Number: LMR16030 Other Parts Discussed in Thread: LM5013 , LM5013-Q1 , LMR38020 , LM5012 Hi.
Here is the schematic:
SX-Texas-01.pdf
Some of the calculations:
------------------------------------ FEEDBACK RESISTORS ------------------------------------ …
Part Number: LMR16030 I've tried using this IC to design 50->12V and 50->5V regulators, but have the same unexpectedly low output from both of them. Rather than the expected voltage, around 400mV is being generated, which gradually decays to 340mV then…
Part Number: LMR16030 Hi,
Regarding the application notes SNVA755 and SNVA489C, I have designed an input filter but i am not sure about component values. As you can see below, like in the SNVCA489C, i did not use an damping electrolytic capacitor and…
Part Number: LMR16030 Hi Team,
Our customer is using LMR16030 regulator to convert 48V TO 3.3V. Initially they used 500KHz as switching frequency. Now they are changing the switching frequency to 1MHz and 2 MHz. He would like to know how much does it affect…
Part Number: LMR16030
Hi support team,
Can the PGOOD pin of LMR16030PDDAR be floating?
Can the SS pin of LMR16030SDDAR be a floating?
If both of the above are possible, is it possible to replace LMR16030PDDAR and LMR16030SDDAR?
Even if the SS of LMR16030SDDAR…
Part Number: LMR16030
Can we use 22uF CHIP CAP+100nF CHIP CAP+220uF DIP E.CAP for the output capactitances of LMR16030?
1, in datasheet of LMR16030,the output capactitance is recommended as 2x47uF CHIP CAP or 1x100uF E.CAP.
According to our actual ccmponents…
Part Number: LMR16030 Can we use 22uF CHIP CAP+100nF CHIP CAP+220uF DIP E.CAP for the output capactitances of LMR16030?
rctan@computime.com
1, In datasheet of LMR16030,the output capactitance is recommended as 2x47uF CHIP CAP or 1x100uF E.CAP.
According…
Part Number: LMR16030 Vout (VS1) in the circuit diagram below is used as the voltage to drive the solenoid. The solenoids themselves will be connected in multiple connections, and they will all be turned on at PWM:20kHz.
We checked the waveform of VSW…
Part Number: LMR16030 Hi,
could you help to comments on whether below SW waveform is normal when LMR16030S work in light load mode.
below is the waveform.
1. does it make sense?
2. the reason that cause the spur before pulse.