Part Number: LMR23610 Tool/software: Hello
Will it operate correctly if the thermal pad of the LMR23610 is not connected? If the thermal pad is not connected, will the thermal shutdown, for example, malfunction? Specifically, the LMR23610 is installed…
Part Number: LMR23610 hello, importing the model into pspice, the simulator reports the error below:
,
Pspice Model: SNVMAT7.ZIP (165 KB) - PSpice Model
How is this problem fixed?
Part Number: LMR23610 Hello, I have several questions regarding Tina and Spice model: LMR23610A Unencrypted Non-Inverting and Inverting PSpice Transient Model
1. When loading the model this message is returned " More than one subcircuit exists or…
Part Number: LMR23610-Q1 Other Parts Discussed in Thread: LMR23615 Tool/software: Hi all,
LMR23610-Q1 datasheet lists formula 18 as follows:
However, the (pin-compatible) LMR23615, 25 and 30 list as follows:
Can you please advice as to…
Part Number: LMR23610LMR23610 will work on PFM mode when light load.
What's the specific relationship/formula between work frequency and output current/input output voltage/inductance value?
Part Number: LMR23610 Hi,
LMR23610 block diagram shows "OV/UV Detector". If OV/UV is occurred on FB pin, what is going on LMR23610? Please let us know.
Thanks and best regards, M.HATTORI.
Part Number: LMR23610 Other Parts Discussed in Thread: LMR23630 We are developing a new product and need a reliable circuit to drive two LEDs (in series) with the Microchip MIC2291 LED Driver. We now have the prototype PCBs in hand but aren’t getting…
Part Number: LMR23610 Hi,
Good Day.
Customer is looking for OTS test socket for the part LMR23610ADDAR. Is there a way he can find out what is used at the CM where it is manufactured?
He's trying to find out the source of the test socket used for…
Part Number: LMR23610 Is there a test socket for the HSOIC-8 package that this device uses? SOIC-8 test sockets do not take into account the thermal pad on the base of the package.