The TI E2E™ design support forums will undergo maintenance from July 11 to July 13. If you need design support during this time, open a new support request with our customer support center.
Part Number: LMR23610-Q1 Other Parts Discussed in Thread: LMR23615 Tool/software: Hi all,
LMR23610-Q1 datasheet lists formula 18 as follows:
However, the (pin-compatible) LMR23615, 25 and 30 list as follows:
Can you please advice as to the correct…
Part Number: LMR23610-Q1
Hi,
I am using LMR23610-Q1 as follows:
Vin= 5.5 to 27 V
Fsw= 2 kHz sync with external clock
Iout = 0.4A
Vout = 5.5V
I am worried about what would happen at Vin_min = 5.5V. What would be the Vdrop across the IC and what Vout whould…
Part Number: LMR23610-Q1 Other Parts Discussed in Thread: LMR23610 , Hello Team, customer needs following configuration but seems it's not possible to do this with webench
I tried to optimize the LMR23610 Design with Webench Power Designer. Unfortunatelly…
Part Number: LMR23610-Q1 Hello, We've been checking the datasheet and it seems that there is no mention of overvoltage protection. Can you please confirm if there's some sort of overvoltage protection included in the device? The customer will be subjecting…
Part Number: LMR23610-Q1 Hi,
Iam using multiple buck converters in my design for generating different voltages.
Can all these buck converters be operated at the same or different frequencies?
I read that when multiple buck converters are switching at…
Part Number: LMR23610-Q1 Other Parts Discussed in Thread: LMR23610 Hello,
I noticed that equation 16 in the datasheet (REVISED APRIL 2017) contains an error 'as I think'
the equation calculates the minimum output capacitor value to have a target…
Part Number: LMR23610-Q1 Tool/software: WEBENCH® Design Tools Hello Webench team,
I would like to confirm the load transient result when output current slew rate is changed any speed.
However, I don't find any input area for changing slew rate.
Could…
Hi John,
Yes, the slow VIN ramp is very suspicious to me. Also your signals look a lot cleaner now. I'm now suspicious of the input circuit.
Do you get the same results if you connect the power directly to the VIN net on LMR23610/LMR23630 in your…
Hi,
Yes according to the datasheet it seems to be ok to keep the EN pin floating.
Another alternative is to use a part where EN can be tied directly to VIN such as
LMR23610-q1 or LM43600-Q1
www.ti.com/.../LMR23610-Q1
www.ti.com/.../LM43600-Q1
T…
Hi Pol
We are familiar with this type of device and we dont have a direct replacement in our product line but TI has this device which may be of interest www.ti.com/.../lmr23610-q1.pdf
I hope this helps
Regards
Peter