Part Number: LMR23625 Other Parts Discussed in Thread: TPS552872 Hey Buck Regulator Team,
I have a customer considering using the LMR23625 for a new project and we were hoping you could provide some feedback and design guidance.
The key requirements are…
Part Number: LMR23625-Q1 Hi experts,
Let me confirm R_thetaJC in datasheet, please.
In the latest version (Revised_March_2018) shows 5.9C/W in DDA package. There is a big difference compared with past version value. Is this value correct? If it is, what…
Part Number: LMR23625-Q1 Hi
Could you help to confirm whether the difference between LMR23625CFPQDRRRQ1 & LMR23625CFPDRRR is only in AEC-Q100 certification, thank you!
Part Number: LMR23625 In our device we have used the part LMR23625CDDAR as a wide input regulator which takes the input from the load dump protection circuit and then gives output to the battery charger IC.
for our compliance test we provide upto 36v supply…
Part Number: LM61430-Q1 Other Parts Discussed in Thread: LMR23625-Q1 , , LMR23625 Hi,
I would like to know what is the diffenence between LMR23625-Q1 and LM61430-Q1. I checked their specification and they seem to be similar, however, I am not sure if my understading…
Part Number: LMR23625-Q1 Hi,
I need help comparing these two devices. I checked the datasheet and it appears to me that the simple switch part is designed for efficiency while the other is for low EMI. Is this all? Can you help elaborate?
Thanks!
reg…
Part Number: LMR23625-Q1 Hi support team.
My customer asked me about the difference between TOC of Q1 and Non Q1 on WSON package
Why is the TOC different between Q1 and nonQ1 on WSON package?
Q1 : 12ms nonQ1 : 10ms
Best regards,
Higa
Part Number: LMR23625 Hi Team,
There is a good new that we DIN LMR23625
And there have one thing need your support! Please help check this SCH & suggest L , THX
Vin = 12V~24V
Vo=5V / Io=3A