Part Number: LMR23625 Hi,
I use the LMR23625CQDDARQ1 in a typical application.
The layout is according to recommendations in DS.
Input voltage = 24V.
Output voltage = 5V
Output current = 300mA.
The DC/DC, L15 and C163 heat up to 55 degrees Celsius.
Please…
Part Number: LMR23630-Q1 LMR23625-Q1 Other Parts Discussed in Thread: LMR23625-Q1 Hi,
We got a question from the customer about LMR23625-Q1 and LMR23630-Q1. Could you help us?
[Question] Could you provide below characteristics of the internal FET? They want…
Part Number: LMR23625-Q1 Hi,
Is there any reference calculation sheet (in excel format) can be provided ??
for example, I have the inductor "COIL 22UH@100KHZ M 74437346220 SMD WURTH PB FREE" on hand, instead of "L2 Inductor, Wirewound, Powdered Iron,…
Part Number: LMR23625 Hi Team,
I'm curious about how the LMR23625 detect the current and go into the hiccup mode? Is it a valley current detection of inductor current within the peak current mode? From the datasheet, I can't figure it out clearly. Hope…
Part Number: LMR23625-Q1 Other Parts Discussed in Thread: LMR23625 , LM76003 , LM76002 Hi,
Now we use LMR23625-Q1 and we need to have my product compliant with ISO-16750-2 (24 V system).
Would you have any suggestion for our check again?
And if have any risk…
Part Number: LMR23625 Dear Team,
I am designing circuits using LMR23625.
My circuit has a external power source and the output is connected to Vout of LMR23625. When Vin=0[V] of LMR23625, Vout(+5V) voltage of LMR23625 is 5[V] by the external power source…
Part Number: LMR23625-Q1 Other Parts Discussed in Thread: LMR23625 , LMR36015-Q1 Hi Expert,
Does LMR23625 could suspport load dump 60V/400mS test? If not, any alternative solution for it? Thanks!
Part Number: LMR23625-Q1 Hello,
My customer was wondering what would happen on LMR23625-Q1 in WSON(12 pin package) at the following conditions. Would you please tell me what would happen or if it might be damaged?
1. NC(#11) short to VIN(#10)
2. NC(#11…
Part Number: LMR23625 Hi Support team
Need verification, I am working on a design for a customer, there is a case where the input maybe 20 and the desired output will be 20v at 3A. Will the device go into pass thru mode, or will something else happen…
Part Number: LMR23625-Q1 Hi,
We got a question from the customer about LMR23625CFPQDRRRQ1(WSON PKG). Could you help us?
[Question] If they don't use PGOOD function, what is the recommended terminal proccecing? Is it ok to be OPEN?
Best Regards, tate…