Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed from November 25 through December 2. Thank you for your patience.
Part Number: LMR23625-Q1 Hi,
We got a question from the customer about LMR23625-Q1. Could you help us?
[Question] They are concerned about that the inductor current ripple disturb a stable current mode operation. They assume when the inductor ripple current…
Part Number: LMR23625-Q1 Hi,
We got a question from the customer about LMR23625-Q1. Could you help us?
[Question] - How much is the variation of Tss=6msec(WSON PKG)? They want to make sure min and max value. - Is there plots of Tss vs Tj characteristic(WSON…
Part Number: LMR23625-Q1 Hi,
We got a question from the customer about LMR23625-Q1. Could you help us?
[Question] They found a distortion on SW node waveform. Please refer to below figure. Why does this distortion occur? They checked the inductor waveform…
Part Number: LMR23625-Q1 Hi,
I received the following question from my customer.
Has the LMR23625-Q1 been verified working on the all operate junction temperature and all Supply voltage?
They don't require guarantee, however they would like to confirm…
Part Number: LMR23625-Q1 Hi,
We got a question from the customer about LMR23625-Q1. Could you help us?
[Question] They are considering using this IC under the following condition.
Vin=3.9V min Vout=3.3V Iout=1A
In this condition, the IC will enter the low…
Part Number: LMR23625-Q1 Hello Team,
I have schematic review about LMR23625-Q1 from customer. I write it down could you check and give me feedback?
I am awaiting your reply
Masayuki,
************
Questions,
-Our customer wants to add 2 ohm resistor between…
Other Parts Discussed in Thread: LMR23630 , LMR23625-Q1 Hi,
Customer of mine is using LMR23625-Q1 in their Automotive Infortainment. They're observing the output voltage drop (from 5V to 1.5V) with this device
Test Condition:
Vin = 12V
Vout = 5V @ 2.…
Part Number: LMR23625-Q1 Hi,
My customer is severely afraid of happening problems by dispersion of characteristics specified only typical value.
Is there any parameters that the dispersion is large(i.e. half/twice)?
Please let me know for our reference…
Part Number: LMR23625-Q1 Other Parts Discussed in Thread: LMS3655-Q1 , LMS3655 , LMR23625
Dear Team,
similar request like my previous post about the LMS3655-Q1 , but the customer has new specs (lower output currents):
V-in = car battery
V-out = 5V
I-load…