Other Parts Discussed in Thread: LMR24210 Hello-
We are concerned about PCB cleaning after assembly of the LMR24210, as there are exposed edges of the die. Are there any limitations or special requirements which should be observed?
Thanks and Best Regards…
Other Parts Discussed in Thread: LMR24210 Noticed in the latest LMR24210 datasheet there are references to a PGND pin; however, after inpsecting the diagram of the ball/landing pattern, I do not see a PGND pin on the part. Is this a typo or am I missing…
To achieve longest battery life should I drive each LMR2410 with 12V (one is regulating to 5V, one to 3.3, one to 1.8, and one to 1.2v). OR should I drive 5v into the 3.3 and 1.8 ans 1.2V regulators. Estimated current draw for each voltage is 200mA? the…
Other Parts Discussed in Thread: LMR24210 Hi,
In the description tab for the LMR24210, the temperature range is quoted as -20 to +125. In the datasheet the junction temp range is quoted -40 to +125... Which is correct ?
Best Regards
Galvanic isolation is provided with a transformer. The LMR24210 cannot be used in any standard topology using a transformer.
Please send more details on what you are trying to achieve so that I can make a recommendation.
Regards,
Marc
Other Parts Discussed in Thread: LMR24220 , LMR24210 , TPS40170 , LM34937 Hello,
Below is a question from a customer if the SS input of LMR24220 can be used as a tracking input. Could you please help the customer out?
Many thanks, Esa -------------
LMR24210…
Other Parts Discussed in Thread: LMZ10501 , LMZ10500 , LMR24210 , LMR24220 1-A power module and 42-V synchronous power regulators are industry’s smallest for point-of-load power conversions
DALLAS (Oct. 10, 2011) – Texas Instruments Incorporated…
We have put the Part into Digikey feed, it will be available within 2 hours so you can proceed witht BuildIt Lite order.
The other alternative is to get a sample order directly from ti website for that part:
Come back to your question about how to force…