Part Number: LMR33610 Hello team,
I have a question about inductor value for LMR33610.
Looking at table 2 on datasheet for 5Vout with 1400kHz, 2.2uH is recommended.
However calculating inductor value with using equation 4 with assuming 24Vin, 0…
Part Number: LMR33610 Other Parts Discussed in Thread: LMR33620 Hi,
Could you please let me know the LMR33610 current limit spec(Max, Typ)?
I don't find the current limit spec in the datasheet....
Thanks
Muk
Part Number: LMR33610 Other Parts Discussed in Thread: LMR33640 , TINA-TI , Hi team,
My customer would like to do a transient analysis of LMR33610. Do you have the LMR33610 TINA-TI software? Or is the LMR33640 PSpice transient model able to be used…
Part Number: LMR33610 Hello exerts,
The following items are not included in the data sheet.
Please tell me.
① Ilimit value ⇒ min, typ, max
② Isc value ⇒ min, typ, max
Thanks and best regards,
Kazuyuki Kamiya
Part Number: LMR33610 Other Parts Discussed in Thread: LMR36510 , LMR33620 Hi TI,
I want use new design LMR33610ADDAR,
Design Requirement is
Input voltage is 30V and Current is 150mA,
and output volatge of buck regulator is 5V and current is 300mA…
Part Number: LMR33610 Do TINA/Pspice simulated rise-fall times of switching pin for LMR336* devices match to actual measured rise/fall times?
In general observation with other manufacturer buck converters we see it does not match.
Is there any method…
Part Number: LMR33610 Hi All!
Can the LMR33610 (or similar) buck converter connect directly to solar panel (5...10...20W) for charging of 12V SLA? Any experience on that? Does the "current source" mode of solar panel affect the operation of DC/DC (buck…
Part Number: LMR33620 Other Parts Discussed in Thread: LMR33610 , LMR33630 Tool/software: WEBENCH® Design Tools We want to get EVM LMR33620 or LMR33610.
Is there any EVM? and can we buy it from TI store?
Part Number: LMR33610 Hello,
A customer of mine is asking about more details on the note on page 5, chapter 7.3 and note 3.
Is it possible to share more details on this topic?
Best regards
Jorgen
Part Number: LMR33610 I'm looking for a footprint compatible part for the LMR33610(B) that doesn't alter it's switching frequency on light loads, but I'm drawing a bit of a blank.
Is there such a part?
Thanks,
G