Part Number: LMR33620 Team,
my customer is using LMR33620 in a new application. There is a possible fault condition where the Vin of LMR33620 is not present, but the EN signal (3.3V) is still present. That means the LMR33620 is unpowered and EN is 3.3V. …
Part Number: LMR33620
Hi,
I have a design with the LMR33620CRNX where input range is 12-18V in, with 5V out, and pretty much a stable 60mA load. The efficiency is around 70%. I really need to conserve power here, so 90% would be a good goal.
ISSUES: Pretty…
Part Number: LMR33620 Hi,
My customer wants the sample 2-layer Layout of LMR33620 QFN package. We can refer 2-Layer Layout on LMR33620 DDA package on the datasheet. But, we can only find 4-layer information of QFN package. Could you please 2-Layer Layout…
Part Number: LMR33620 Other Parts Discussed in Thread: LMR33630 Hello,
I'm looking for the equivalent part of ISL854102. https://www.renesas.com/us/en/document/dst/isl854102-datasheet?r=529066
The most important requirement is fast load transient response…
Part Number: LMR33620-Q1 Hi Team,
There is a good new that we could DIN LMR33620-Q1!
Regarding the Tj formula, what worst case conditions are considered by the Datasheet? THX For example: component error, aging, temperature deviation (125) ℃...etc
Part Number: LMR33620-Q1 Other Parts Discussed in Thread: LMR33620 Hi all,
My first question is in general about the TI categorization and how to use this inside a safety project. There is the split into different levels of functional safety capabilities…
Part Number: LMR33620 Other Parts Discussed in Thread: LMR33630ARNXEVM , LMR33630CRNXEVM Hello,
I have a customer who is interested in using the LMR33620BRNX (1.4MHz) and is asking the following:
Their output is 5V @ 1A, Do we have any data on the temperature…
Part Number: LMR33620-Q1 Dear Specialists,
My customer'd like to know the difference between LMR33620BQRNXRQ1 and LMR33620BRNXR.
I think the difference is test specs because Q1 is for qualifying AEC-Q100 and the same die is used inside.
Is it correct…
Part Number: LMR33620 Other Parts Discussed in Thread: LMR33630 Dear Team,
Do LMR33620 and LMR33630 have force PWM mode?
If yes, how could I set chip into force PWM mode?
Many Thanks,
Jimmy
Part Number: LMR33620 Other Parts Discussed in Thread: LMR33640 Hi Team, Our customer would like to confirm if 2 LMR33620 can be connected in parallel to increase the current as they need a current value of 4A? They have LMR33620 as of the moment so if it…