Part Number: LMR33630 I want to simulate LMR33630 in webench but webench responds with "Hmm we found LMR33630 but it is not supported in this tool". Am I doing something wrong?
Part Number: LMR33630 Hi team,
I would like to ask a question. The datasheet of LMR33630 is about 9.2.2.5 Output Capacitor Selection. There is the following description. I would like to confirm the values of ΔVout and ΔIout?
Thanks
Li…
Part Number: LMR33630 Good Morning/Afternoon.
Sorry to disturb you but I need to ask an information.
Is availalable some data about LMR33630 no-load input current?
In particular both typical and maximum.
I know that some information could be extracted…
Part Number: LMR33630 Hi Team,
May I check with you if we have a tolerance level for the specs below as labeled "d" and "e"?
For example d - 1.27 , e - 3.81. Do we have a min and max specs for this ?
Thanks!
Best Regards,
Ern…
Part Number: LMR33630-Q1 Hi Sir,
We knew the electrical characteristics of the datasheet that provided typical values at TJ = 25°C, my customer is asking for how to calculate the 3.3V-out tolerance range at TJ = -40C ~ +85C. If the LMR33630AQRNXRQ1…
Part Number: LMR33630 Hi Expert
I will be very grateful if you can answer my question
Q1. Does PSPICE transient Model support to estimate Gain / Phase Margin ?
Q2.Can expert guide me, how to using PSPICE tool to setup the GM/PM simulation about the…
Part Number: LMR33630-Q1 Other Parts Discussed in Thread: LMR33630 Hi team,
My customer would like to know what kind of materials are included in the LMR33630? would you please any document explain this?
BR
Jimmy
Part Number: LMR33630-Q1 Other Parts Discussed in Thread: LMR33630 Hi team,
Please answer the following 33630B questions: Now the customer tested that LMR33630-Q1 can still work when EN is floating; does EN default to high? They test the result (SW/EN…
Part Number: LMR33630 Van you please Check my Design, if i use 12V vin i do Not get any Output voltage. If I put 5,8V as VIN the power LED's starts to light.
thank you for help. I need 5V , 3.3V , 1.5V , 1.02V
The 5V should work first. I used your…