Part Number: LMR34215-Q1
Hi,
I am designing converter for following specification -
Vin nominal - 12V
Vin min - 11.76V
Vin max - 12.24
Iout - 300mA.
Vout - 5.6V
1. Using the Webench Designer I got the circuit and while validating it with equations provided…
Part Number: LMR34215-Q1 Other Parts Discussed in Thread: LMR36015 Hi TI,
Could you please help me find a replacement for LMR34215FAQRNXTQ1 with the same pinout and same package/case.
I have used this in my design and now it is out of stock everywhere.…
Part Number: LMR34215-Q1 Other Parts Discussed in Thread: LMR33620 , LMR43620 , LMR33610 , LMR36015 Hi,
My Requirement is 6V-36V Input, 5V Output, 1A Output, Ambient Temperature is (-40degC to 90degC). Can you please suggest any part which meets all this…
Part Number: LMR34215-Q1
Team,
Due to shortages I need to switch from a 2.1Mhz version of the LMR34215 to a 400khz version of the part. In order to avoid PCB changes we need to use a 12uH inductor instead of 15uH specified in datasheet.
I need to understand…
Part Number: LMR34215-Q1 Other Parts Discussed in Thread: LMR33630-Q1 , LMR33620-Q1 Hi,
I have some questions regarding the devices LMR34215 and LMR34206 with 5V output and no FPWM:
Would they both work under the same output inductor and capacitance? I…
Part Number: LMR34215-Q1 Hello Guys,
Good day.
Our customer exported the TINA project file from WEBENCH circuit, but when he tried to run an Analysis, he encountered the attached error message.
Is there any special configuration in simulation parameters…
Part Number: LMR34215-Q1 Dear team,
Our customer is going to use this device by the 9V output. Therefore, we choose a device of 400kHz. As for the device of 400kHz, "Spread spectrum" is No, will you meet CISPR25 class 5 standard?
Best Regards…
Part Number: LMR34215-Q1 Other Parts Discussed in Thread: LMR33630-Q1 , LM5060
Hi,
Our customer requests an example circuit using TVS and two layers layout data. Then, our customer needs standard are "CISPR25 class5" and "JASO D-1,D-2".…