Part Number: LMR36006-Q1 Other Parts Discussed in Thread: LMR36006 Hello Team,
I am using LMR36006-Q1 buck IC for converting 12V to 5V. So, i am using suggested Inductor & capacitor values in my schematic.
But how to get the load transient values…
Part Number: LMR36006-Q1 Hello,
I would like to ask you a question about LMR36006-Q1. RNX0012B and RNX0012C have information on EXAMPLE BOARD LAYOUT and EXAMPLE STENCIL DESIGN in the data sheets, but there are some differences. It also states that the…
Part Number: LMR36006-Q1 Other Parts Discussed in Thread: LMR36006 Hello Team,
I need the FIT ratings of the LMR36606-Q1 IC. Where can i get these details.
Thanks and Regards,
Giridhar.
Part Number: LMR36006-Q1 Hi,
I am having an issue with the part LMR36006FSC3RNXTQ1.
I am using it to lower the 24VDC voltage to 3.3V and 0.15A.
I am measuring a case temperature of 70C with ambient temperature of 25C.
I have looked into the Flip…
Part Number: LMR36006-Q1 Hello Team, enclosed a simulation which do not fit do real measurement. Please could you help to optimize it. Many Thanks Josef
---
Our simulation schematics is as below.
Simulation results are as below.
1)Inductor…
Part Number: LMR36006-Q1 Other Parts Discussed in Thread: LMR36006 Hi Sir,
Please help confirm below schematics, and response need modify suggest,thanks!
LMR36006 5~32V to 3.3V
Part Number: LMR36006-Q1 Other Parts Discussed in Thread: LMR36006
Hi expert,
LMR36006 has 2type package infomation in datahsheet. It seems to have difference about hight.
RNX0012B VQFN-HR - 1 mm max height
RNX0012C VQFN-HR - 0.9 mm max height…
Part Number: LMR36006-Q1 Other Parts Discussed in Thread: LM46000-Q1 , LMR36006 Hi,
I am working on a design to covert 12/24V DC battery to 6~7V, then through a LDO to 5V to power a MCU. I find out that both LMR36006-Q1 and LM46000-Q1 meet the requirement…
Part Number: LMR36006-Q1 Other Parts Discussed in Thread: LMR33630CRNXEVM Hi, I tested my design with the eval board LMR33630CRNXEVM. Since I wanted to test it with the LMR36006AQRNXRQ1, I changed the original controller to this one. Moreover, I changed…