Part Number: LMR36015-Q1 Other Parts Discussed in Thread: LMR36015 Hi Team,
In the case that SW voltage is higher than Vin accidentally(like reverse connection), How much current can LMR36015 withstand with no damage? Do we need to put diode at Vin line…
hi, Kiran,
If the normal input voltage is 36V I suggest a 60V grade buck and leave some buffer.
LMR36015-Q1 4.2-V to 60-V, 1.5-A ultra-small synchronous step-down converter
LMR38020-Q1 Automotive SIMPLE SWITCHER® power converter 4.2-V to 80-V, 2-A, synchronous…
Part Number: LMR36015-Q1 Hi Team,
do we have a reference design / layout for the LMR36015-Q1 that has been tested to CISPR25 Class 5 compliance?
Thanks and Regards,
Mihir
Part Number: LMR36015-Q1 Other Parts Discussed in Thread: LMR36015 Hello,
I have a problem with the 400kHz regulator regarding the overshoot on the switching node.
The 2100kHz regulator has better regulation behaviour, but has an other problem, the package…
Part Number: LM25010-Q1 Other Parts Discussed in Thread: LM5160-Q1 , LMR38010 , LM5013-Q1 , LM5012-Q1 , LMR36015-Q1 , LMR38010-Q1 , TPS54140 , LMR38020 , LM5013 , LM5012 , LMR36015 , LMR36015AEVM Hi to all,
Until now we were using the LM25010-Q1 part but we are…
Part Number: TPS2375 Other Parts Discussed in Thread: LMR36015-Q1 , LMR36015 , , LM5010 , PMP10812 , TPS2378 , , Hi, I need some input from a TI power supply FAE expert: I need a PoE PD solution for a device where size and (most importantly) height are the major…
Part Number: TPS54360 Other Parts Discussed in Thread: LMR36015
Hi TI team ,
We are using the chip TPS54360DDAR for generating -24V input from +24V .Recently we have observed from field that TPS54360DDAR is Burning .its burning at Vin Pin (Pin no 2) and…
Part Number: LM5143-Q1 Other Parts Discussed in Thread: LMR36015-Q1 , LM5145 , LM5146-Q1 , LMR36015 , LM5160 , LM10011 I would like to use LM5143-Q1 in an application that:
1) VIN = 48VDC
2) Adjustable VOUT = 0.6V .. 47V @1.25A
My questions are:
1) Is LM5143…
Part Number: DRV8305 Other Parts Discussed in Thread: LMR36015-Q1 , , LMR36015 Originally a DRV8305N was used on a board design but it got switched to a DRV83053 variant.
The Vreg pin (outputs 3.3V from the DRV internal LDO) is connected to our boards switching…