Part Number: LMR36015 Other Parts Discussed in Thread: BQ25302 , Tool/software: Hi everyone, I mounted the LMR36015BRNX step-down converter on a 4-layer PCB. It is a handheld device equipped with a single lithium polymer cell.
During the usual CE EMC measurements…
Part Number: LMR36015-Q1 Tool/software: There are two packages listed in the data sheet for this device: ``RNX0012B'' and ``RNX0012C.'' Which is the "LMR36015FSC3RNXRQ1" package?
Part Number: LMR36015 Tool/software: Hello everyone,
I need to simulate the LMR36015 on a different simulator (SIMetrix) but it's engine it completely based on PSPICE, but when I add the .lib on this simulator and run the simulation it appear an error…
Part Number: LMR36015-Q1 Tool/software: I want to know the LMR36015-Q1 maximum transient voltage in ISO 7637-2 pulse 1&2a&3a&3b for a 24V system, as shown in other product figure below
Part Number: LMR36015 Tool/software: Hi,
This is regarding MPN - LMR36015FSCQRNXRQ1.
I captured the waveform of Inductor Current & Voltage across the switch.
My Doubt is:
1. I am seeing some weird behavior of Inductor Current while ramping up. As…
Hi Kaushalya,
Thank you for the info. I agree with you on the sim time, and I would run a line transient test for more convincing evidence of performance. By the way, 40mV ripple is not bad for a 3.3V output, and hope this meet your spec.
Thanks,
You…
Part Number: LMR36015-Q1 Hi ,
This is regarding MPN - LMR36015FSCQRNXRQ1.
Can you please provide the current capability of Power Good (PG) Pin.
.Regards,
Ajay
Part Number: LMR36015-Q1 Hi ,
This is regarding MPN - LMR36015FSCQRNXRQ1. The .lib file available in the website is not working for Ansys tool.
Can you please provide me the common .lib file which will work for every tool.
& One more thing that while simulating…
Part Number: LMR36015-Q1 Hi TI expert,
May I know whether LMR36015-Q1 has any OVP mechanism?
I notice we do have current limit and minimum on-time requirement.
So if the OVP do happen on Vout side, the controller will only reduce the PWM & frequency until…
Part Number: LMR36015 Hi,
I have my design with LMR36015 quite advanced and I would like to have a feedback from TI.
Attached you will find a document with a description of the stack, sch, and layers.
There is a point, pin12 - SW node, where I would like…