Part Number: LMR36015-Q1 Hi ,
This is regarding MPN - LMR36015AQRNXRQ1 . I tried simulating the circuit with PSPICE Model for following data.
Input - 6V-36V
Output - 5V, 1A
Switching frequency - 400KHz
I got some issues that while simulating I am getting…
Part Number: LMR36015-Q1 Other Parts Discussed in Thread: LMR36006-Q1 , LMR36015 , LMR36006 , LMR36015S , We measure LMR36015FSCQRNXTQ1 case temp at room temperature and would like to find out if running it at 80°C ambient would maintain junction temperature…
Part Number: LMR36015 How can I get access to the old Webench from 2021?
I designed a power supply using the LMR36015 using it. When I tried to analyze that circuit again Webench now says it isn't supported. It was supported in 2021!
This is crazy…
Part Number: LMR36015 Other Parts Discussed in Thread: LV2862 ,
Hi there, We need an IBB solution that can go from +13-14V to -12V. The current requirements are ≈50-100mA (or less). My understanding was that most "typical" buck controllers could be used…
Part Number: LMR36015 Hi TI expert,
The function of the capacitor between BOOT and SW is providing voltage for internal high-side driver. In the start time, If the high-side tube is turned on first, how does it turn on when the capacitor is no voltage? …
Part Number: LMR36015 I Use LMR36015 to realize the voltage conversion from 50V to 7.3V, but w hen I use "PSpice for TI" software for simulation, the total simulation time is 300ms, but when it reaches 100ms, the simulation is stuck and cannot be completed…
Part Number: LMR36015 HI there,
Does the industrial version of this part have Spread Spectrum? It's in the splash summary but I couldn't find it anywhere else in the datasheet? Looks like it could only be on the automotive part?
Thanks!
Part Number: LMR36015S Hi
The customer has a question they are testing the HOT-PLUG,
The voltage will exceed 60v and burn the LMR36015S ,
do you need to suggest adding hot swap?
Part Number: LMR36015S Figure 10-4 of the current datasheet shows efficiency down to 1mA.
Do we have any data for lower currents? We'd like to see 24V in, 5V out efficiency at 10uA load (or the equivalently, input/quiescent current under those conditions…
Part Number: LMR36015 We are currently using LMR36015BRNXR/BRNXT on our desings, When we change it to LMR36015FBRNXR/FBRNXT the power looses on the chip goes up by about 0.5W -
All we have done is just replace the chip on the board and left all other…