Part Number: LMR36506-Q1 Other Parts Discussed in Thread: LMR36506 Hello,
I am using the LMR36506 in a very critical power consumption application.
Our input voltage is 9V and our output voltage is 1V8. Our circuit is as follow:
We measured a quiescent…
Part Number: LMR36506-Q1 Hello Expert,
Our customer is considering to use LMR36506-Q1. Then, we have questions for this device.
They are selecting external components for this device. Regarding CVCC, I understand that suggested 1uF is including variation…
Part Number: LMR36506-Q1 Hi team,
One of my customer is using LMR36506MSCQRPERQ1.
It will work with PFM mode when the output goes low.
1. Are there lower limit of switching frequency in PFM mode?
2. How much is the on-time in PFM mode? Also, is it fixed…
Part Number: LMR36506 Other Parts Discussed in Thread: LMR54406 , LMR33610 Hello TI,
we want to convert 14V input voltage to 1V output voltage using LMR36506 (LMR36506RRPER, adjustable fsw, PFM mode). The output load can vary between 40 mA and 100 mA. …
Part Number: LMR36506 Datasheet mentions if EN pin voltage is above 0.4v then IC wakes up, but there is another tab Ven_Vout : 1.6V to 1.36V with typical 1.263V
which one of this is true ?
When V_EN goes above 0.4 IC Wakes up does it start switching …
Part Number: LMR36506 Hello Team,
maybe there is an error in the data sheet, page 32: in the formula for calculating Rent there is Ven-h which is not defined.
Maybe this should read Ven-out?
Thanks and Best Regards, Hans
Part Number: LMR36506-Q1 Hi team,
I got some questions about efficiency of LMR36506-Q1.
1. There are some efficiency data graph on D/S including page#1.
Do these data indicate the efficiency of IC or efficiency of the circuit?
I assume that it must be…
Part Number: LMR36506-Q1 Other Parts Discussed in Thread: LMR36506 Hi team,
Could you specify in more detail that the difference in between LMR36506 industrial grade and automotive grade(-Q1). Their temp range are all the same.
Thanks.
Regards,
Ale…
Part Number: LMR36506 Hi. I´m doing some Tests with the LMR3650RREVM and I have some questions. In the Datasheet of LMR36506 I found out that " Which mode the LMR36506 operates in, depends on which variant from this family is selected ". That…
Hi Amber,
LMR36506 can also work, but I suspect a large portion of this will be due to your input filter, as seen in both the LMR36506 and LMR36006. Honestly, based off of the test result, it may be easier to pass with the LMR36006 from the EMI waveform…