Part Number: LMR36506-Q1 Hi, Good day. Our customer is using the LMR36506-Q1 and they have this inquiry: I would like to know what the quiescent current draw is for the LMR36506-Q1 when in standby mode (i.e., VIN less than turn-on voltage) with a turn…
Part Number: LMR36506-Q1 Other Parts Discussed in Thread: LMR36506 Hi team,
Now my customer is going to use LM36506-Q1 with 50-60V input. In the case of this level of input voltage, the switching frequency is reduced to around 1.3MHz by frequency foldback…
Part Number: LMR36506-Q1 Hi, team.
My customer is considering to use this device with VIN=50V and EN=13V. Customer understand the switching frequency is folded back due to the high VIN voltage and it's no problem.
In their plan, EN will be forced…
Part Number: LMR36506-Q1 Hello,
I am looking at the LMR36506-Q1 for an application targeting an output voltage of 24 V at 0.5 A max. I've attached the Webench design here:
https://webench.ti.com/appinfo/webench/scripts/SDP.cgi?ID=4F9012D9EE5EDAFD …
Part Number: LMR36506-Q1 Hi team,
I plan to pull up MODE pin to set Auto mode.
Should I pull it up to VOUT (3.3V use case) or VCC?
Is there any concern if I pull up either of the supplies?
*MODE pin is connected to VCC on top of the datasheet simplified…
Part Number: LMR36506-Q1 Other Parts Discussed in Thread: LMR36506
I have a problem with the 3.3v buck regulator not getting up to correct voltage but appears to deliver 1v.
Chip is LMR36506MSC3RPERQ1 which has fixed 2.2 MHz switching frequency and…
Part Number: LMR36506-Q1 Hello Team,
I used LMR36506MSC-Q1_PSPICE_TRANS model for pSpice and changed Vin to 48V and Vout to 30V. I connected a 400kHz signal (0...3.3V, rectangular) to MODE/SYNC pin but the part does not sync to it. Why?
Thanks for your…
Part Number: LMR36506-Q1 Hi,
Is it save to apply a voltage to the output pins (SW, VOUT/BIAS/FB) of the LMR36506-Q1 and also apply a clock signal to the SYNC pin, while there is no voltage applied to VIN?
Current flow from the output (SW) to the input…