Part Number: LMR36510 Could you please let us know what is the difference between LMR36510ADDAR and LMR36510FADDAR? As mentioned in one of TI's forum ,i.e., FPWM and non FPWM is the difference between them. Could you please let us know what is the difference…
Part Number: LMR36510 Hi Power Management Team,
The Θ JA value for that package is quoted as 42.9°C/W. Θ JC(bot) is quoted as 4.3°C/W, I’m assuming that somewhere in between those two numbers there is a real thermal resistance based…
Part Number: LMR36510 Dear team,
If I want to increase the light low mode efficiency, I can increase the FB resistor value to reduce the loss.
According to the datasheet REBT can be 1M ohms, but is there any concern to increase REBT to 1M ohms.
I know…
Part Number: LMR36510 Hello,
My customer is using LMR36510ADDAR under the conditions below.
- VIN=48V / VOUT=5.1V / Inductor=4.7uH / COUT=10uF/16V/1608/+-20%/X6S
If the capacitance of COUT changes because the COUT capacitor's temperature rises above…
Part Number: LMR36510 Hi,
I am trying to export LMR36510 Webench power designer schematic to TINA TI. But if fails to export. I tried manually adding Spice macro of LMR36510 to TINA TI. But simulation does not work.
LMR36510 Power Supply.TSC
Thank you…
Hi Anuraj,
TI has many LDOs that would be perfect for your application. I have filtered a list at the link below.
Most all devices are RoHS compliant. Look at the Packaging Information page at the end of the datasheet for the info on each orderable part…
Part Number: LMR36510 Hi Sir,
Pls help for below questions? thanks.
What diferentt between LMR36510 F ADDAR and LMR36510ADDAR?
Pls kindly help review schematic as below. Another, we measured PG pin is low, is correct?
Thanks, Ian.
Part Number: LMR33620 Other Parts Discussed in Thread: LMR36510 ,
I'm using LMR36510, but it seems it is out of stock. So I decided to replace it with LMR33620 that I've got from sample. After I assambled it to my board and turned on the PSU the…
Part Number: LMR36510 Other Parts Discussed in Thread: TPS5430 Hi Team,
My customer used LMR36510 in old project and he would like to use LMR36510 to generate negative voltage(-15V), could team help comment below question?
1. There is a app. note that…