Part Number: LMR36520 Hello Support team,
My customer ask what Delta VOUT and Delta IOUT on 9.2.1.2.4. Could you support?
I assume that
Delta IOUT: load transient peak to peak, min to max or max to min
Delta VOUT: customer required voltage change when…
Part Number: LMR36520 One question about application.
if Thermal shutdown and short current are happened at the same time, how is the device behavior? Does IC go to retry mode? if yes, it should have safety concern, right?
Hi Sruthi,
Since there is no update for 4 weeks, may I assume the issue is resolved so I can close the thread here? You can re-open it by adding a new post.
Thanks,
Youhao
Part Number: LMR36520 Hi team,
In synchronous rectification, the peak currents flowing through the two MOSFETs are equal, which is the maximum value of the inductor current.
The current tolerance of the lower tube is smaller than that of the upper tube…
Part Number: LMR36520 Hi,
When I design an islolated fly-buck using the LMR36520, I read the following article as the reference:
Designing an Isolated Buck (Fly-BuckTM) Converter using the LMR36520 (Rev. A) (ti.com)
But I can't understand how the (2D/…
Part Number: LMR36520 Hi.
I have a buck converter design with LMR36520FADDAR.
The designed input voltage is between 17V to 65V.
The designed output voltage is 5.15V, 10 Watt.
The problem is, that there are a voltage spikes at the output with a frequency of…
Thank you, Andrew.
Please let me know once the formula in the app note " Designing an Isolated Buck (Flybuck) Converter using the LMR36520 " is fixed. Thank you.
Part Number: LMR36520 Hi All,
is it possible to add UVLO on IBB only with two resistors ? ( we don't need to drive the EN pin form MCU)
Vin=24V
Vout=-9V
UVLO 11.25V (no hysteresis needed)
Br,
D.
Part Number: LMR36520 we have a PCB with LMR36520ADDAR IC on it .
is it possible to replace this IC with LMR36520FADDAR without changing the PCB and electronic components ?
Part Number: LMR36520 Hi Experts,
Should we connect PGND and Thermal PAD together? It seems not information on the datasheet indicating so.
Regards,
Uchikoshi