Part Number: LMR38010 How should I connect LTC6908-1 clock output to LMR38010 RT/SYNC input?
I find datasheeet figure 8-5 misleading or maybe I don't understand it.
If I treat LTC6908-1 as a low impedance source then according to the datasheet I would…
Part Number: LMR38010 Other Parts Discussed in Thread: LMR38020 Hello,
I wanted to design a buck converter using this IC. I have done the designing part and now i want to simulate the design. I was not able to find the PSpice Model for this IC. May…
Part Number: LMR38010 Hi team,
Regarding the output capacitor for "LMR38010FDDAR," could you please advise on the following points?
If a larger capacitance than the recommended value calculated by WEBENCH is used, are there any risks other than…
Part Number: LMR38010-Q1 Dear TI experts,
Can I get a Pspice transient model of LMR38010S-Q1?
There is only a model of LMR38010S-Q1 in TI.com.
Please check this issue. Thanks.
Best regards,
Chase
Part Number: LMR38010 Tool/software: Hello Expert,
I am using LMR38010 for designing Buck converter from 11.5V to 36V to 10.5V output @ 1A .
Switching frequency : 700KHz, Inductor used 47uH.
Max inductor current is around 1.2A. (Delta IL of 0.2A…
Part Number: LMR38010 Tool/software: Hello Team,
We have connected a diode PMEG10020 before the Feedback on the LMR for SCG protection.
Open points from our side
what is the power dissipation will increase during dead short to ground. and also…
Part Number: LMR38010-Q1 LMR38010FSQDDARQ1 Failure Observation
We observed failure (short circuit) of two LMR38010FSQDDARQ1 devices.
Initially, the EN pin was directly connected to the VIN pin, and the circuit operated without any issues.
Later…
Part Number: LMR38010-Q1 Other Parts Discussed in Thread: LMR38020-Q1 , , LMR38010 , LMR38020 Hi team,
LMR38020-Q1 has the excel sheet which calculates the parameters of peripheral parts, the bode plot and power efficiency. Does LMR38010-Q1 have similar…
Part Number: LMR38010-Q1 Other Parts Discussed in Thread: LM5088-Q1 , LMR38010 , LMR36506-Q1 , LMR36506 Hi team,
My customer has a few questions regarding LMR38010-Q1. Could you please kindly help me answer them?
May I know if TI prepares the excel…
Part Number: LMR38010 Other Parts Discussed in Thread: LM65635 , LMR38020 , LM65625 I designed a PDLC film driver based on SDAA0033 "DC to AC Conversion with DC to DC Buck Converters for PDLC Displays". It isn't working the way I expect so I have some…